A very special vehicle
Standing in the driver's cab of the bright yellow railcar now is Peter Gerber, the SBB Technical Project Manager responsible for its procurement. His eyes gleam, and his voice resounds with enthusiasm when his turn comes to answer questions on the vehicle known, somewhat blandly perhaps, as the 'Xem 181 011': “No doubt about it, this vehicle is certainly very close to my heart,” he says, “I've been working on the project right from the ITT stage.” Harsco Rail had responded to the invitation to tender with a winning design which has now been turned into reality. The design concept tailor-made by Harsco engineers to SBB requirements is packed full of impressive technical features – including automatic clutches at both ends and compatibility with the European Train Control System (ETCS) standards.
“But the most special feature is the hybrid traction system,” says Gerber. “We can drive under electrical power or diesel power. The train driver can switch from one to the other with ease, even without stopping.” Gerber points to two buttons on the control console: one is marked E (for electric), and beside it is a button marked D (for diesel) which is illuminated, indicating that the train is being powered by the mtu PowerPack – as it will be for most of the day. In everyday use, this will rarely be the case: “We're assuming that we will use diesel mode for around 400 hours per year,” explains Gerber. Most of the time, the vehicles will be traveling under overhead power lines. Only if these fail or have to be powered down for maintenance purposes will the mtu PowerPack swing into action right away from its ever-ready standby mode.
On safety duty
The 57 km long Gotthard Tunnel is not just set to be the world's longest railway tunnel, but the safest too. And a lot of effort is going into this. In addition to fire-fighting and ambulance rolling stock, which are also fitted with mtu traction systems, SBB is procuring a total of 13 maintenance railcars and 18 engineless tenders with a variety of technical design-finishes for use in this record-breaking tunnel. The first of these vehicles is due to go into service at the beginning of 2017. Their main task will be to inspect and maintain the tracks, catenaries and other rail infrastructure deployed in the tunnels: “Lighting, ventilation systems, safety installations and radio systems all have to be checked continually,” explains Peter Gerber. This even includes regular rinsing out of the huge drainage shafts: “to prevent stalactites from forming.”
Nocturnal logistical feats
Each weekend sees one of the two tunnel tubes close at night. Once that happens, there's no hanging around: “A total of three trains are brought at high speed – up to 100 kph – from the SBB Maintenance & Intervention Centers in Erstfeld in the north and Biasca in the south. Each train is made up of three to four maintenance railcars with tenders in between, and takes up its position at a different location in the tunnel.” Gerber refers to this as 'time-optimized dispatch' within the tunnel: In order to make the best use of time available within the tunnel, the teams of up to eight people per maintenance car work simultaneously at different locations. At the end of the shift, the individual cars reunite into trains, and another technical gem of the 'Xem 181' comes into play: “A lead car is able to take control of others attached to it,” explains Gerber.