STORY Rail

An uphill task

Posted on August 31, 2015, Images by Dave Nicol

mtu repowered the Alstom diesel-electric Type AD16 locomotive, which transports passengers and various other things in Madagascar
Tomasina, Madagascar

It transports passengers,  fuels, wood, textiles and foodstuffs: the narrow-gauge railroad stretching from the international port of Toamasina to the City of Antananarivo, located some 700 km away on the Madagascan plateau, is the country's principal transport artery, and spine of the Island’s economy.

The railroad is a tough call for locomotives and their drive systems: it would take 10 to 12 hours to ascend the 33 per mille incline. "That's a gradient that goes well beyond the scope of European load profiles," said Dave Nicol, rail applications specialist at mtu South Africa.

Madarail, Madagascar's national rail company, is especially proud of its Alstom diesel-electric Type AD16 locomotive that was repowered using mtu's 'repower kit' in 2013. That gave the locomotive a new lease of life, and can handle the slopes with athletic ease. The scope of supply covered everything needed to integrate the engine into the locomotive – from the generator flange and switchgear cabinet to the complete automation system (comprising ECU 4, PAU Engine and PAU Traction), and all mechanical and electronic engineering services, as well as refurbishing the Alstom alternator.

The repower kit was devised by Peter Pfitzke, project leader, and Werner Knoll, application engineer. Working together with Dave Nicol and his mtu South Africa’s Application Engineering colleagues, they supported Madarail staff throughout the rebuild measure, which took just 7 months. Since Madarail staff had limited experience of high-tech drives, success very much depended on them forming a close-knit team.

Even today, the mtu rail experts in South Africa and Friedrichshafen are in constant touch with the Madarail. They see the Repower Kit as the potential key to other repowering projects in Africa. "The need is definitely there – particularly in view of the number of Alstom locomotives in service throughout Sub-Sahara Africa," said Peter Pfitzke. In the UK too, ten locomotives have been repowered using the kit.

The content of the stories reflects the status as of the respective date of publication. They are not updated. Further developments are therefore not taken into account.

Point of contact

Dave Nicol
Phone:
+27 11 570 4901
E-mail:

Related stories

Rail

"We could already be saving 90% of CO₂ today – but we prefer to discuss it."

A conversation with Dr. Olaf Toedter (Head of New Technologies and Ignition Systems at the Karlsruhe Institute of Technology) and Jörg Schneider (Head of Sustainability at DB Cargo) about HVO, eFuels, and the technologies that no one can see yet.

Read more

Rail

Cruise Train on rails

Superlative in every respect, the Train Suite Shiki-Shima is powered by electricity generated by two mtu Series 4000 engines on non-electrified routes.

Read more

Rail

Special Purpose Railway Vehicles

Read more