STORY Power Generation

Because it has to be really clean: That's why Vetter relies on dynamic uninterruptible power supply

Posted on October 23, 2024 by Lucie Maluck

If the Vetter pharmaceutical company lost power, entire batches of medication would have to be disposed of. mtu Kinetic PowerPacks prevent this.
mtu Kinetic PowerPacks
Find out more about dynamic uninterruptible power supply with mtu Kinetic PowerPacks
Read more
Power outages are part of everyday life in Germany - with serious consequences for the economy. According to a survey by the German Chamber of Industry and Commerce, 42% of the 1,000 companies surveyed from various sectors and regions experienced power outages of up to three minutes in 2023. The consequences are sometimes serious - but not for the German pharmaceutical company Vetter. The company, which has production sites in Germany, Austria and the USA, does not manufacture any medicines itself. Instead, it specializes in filling them aseptically, for example in syringes, cartridges or vials. To ensure that this is completely aseptic, Vetter has been safeguarding its production processes with uninterruptible power supply systems - Kinetic PowerPacks for short - for almost 20 years.  

"A power failure would mean that we would have to dispose of entire batches of medication," says Kai Schumacher. He is Head of Electrical Engineering at pharmaceutical service provider Vetter and, together with his team, ensures that the electricity always flows at Vetter. And always really means 100 percent. "The smallest outages would have the biggest impact," he explains.  

This is because the medicines must be filled in a completely sterile atmosphere. This is required by both the regulatory authorities and Vetter's customers: the largest pharmaceutical manufacturers in the world. No microorganisms or impurities are allowed to get into the active ingredients, as this would compromise their effectiveness and therefore patient safety.  

The Vetter production employees - all wearing overalls, a cap over their hair and a face mask and gloves - therefore fill the medicines in a so-called clean room. The air here is cool and clean, almost sterile smelling. A quiet, constant humming of the filter systems can be heard. The lighting is bright, but not dazzling, and the floor is spotless.

The Ravensburg-based family business Vetter has matured into a global player. Employees fill medicines in so-called clean rooms. To ensure that these cleanrooms are really clean, mtu Kinetic PowerPacks safeguard the power supply.

Ventilation system guarantees sterility in the cleanroom

No germs are allowed to enter the cleanroom. Air flows and air exchange rates are strictly regulated. A ventilation system ensures a constant positive pressure in the room so that it remains sterile even when doors are opened. If the power, and therefore the ventilation system, fails for just a few seconds, sterility in the room can no longer be guaranteed. "Then we would have to dispose of the batches of medication that we are currently filling," explains Kai Schumacher.  

The 30-something has been with Vetter for six years and is rarely seen in the cleanroom. His home is a few stairs away in the company's "technical cellar". This is where he has once again had mtu Kinetic PowerPacks installed. "Because they simply work well," he says.  

mtu Kinetic PowerPacks: Kinetic mass storage ensures constant availability

What makes them special is that they are immediately ready for use even without a battery and can compensate for the smallest irregularities in the power grid. For this purpose, mtu Kinetic PowerPacks have a constantly rotating kinetic mass storage unit. This is coupled with an mtu combustion engine and a synchronous generator which, depending on the operating mode, is also motor-driven and thus compensates for the power factor of different consumers.

As long as the public power grid is running, the kinetic mass storage device - in this case a flywheel - is driven by the generator, which works as an electric motor in this operating state. The heavy kinetic mass storage serves as an "energy battery" that stores the energy and then makes it available when the power fails.  

Youtube Video

The whirring of the flywheel can be heard loud and clear in Kai Schumacher's "technical cellar". You can't have a conversation next to it. But that's the way it should be, because the system has to be ready for use at all times and the kinetic mass storage units have to be running.


Rotational energy starts mtu diesel engine in mtu Kinetic PowerPacks

Things get really exciting when the public power grid fails: part of the energy stored in the flywheel then drives the generator, which then takes over the power supply. Meanwhile, another part of the stored rotational energy helps to start the 12-cylinder mtu Series 4000 diesel engine very quickly. It reaches its rated power within a very short time and can now take over the power supply via the generator and stabilize the flywheel. This happens without interruption - hence the name "uninterruptible power supply".

mtu diesel engine

Complying with the latest emissions standards; preheated; quick start and not running during conditioning mode pre-lubricated.

Synchronous machine

Four-pole synchronous machines from world-renowned manufacturers designed not to exceed Class F temperature rise; right-sized for your application and to absorb load harmonics.

Kinetic energy module

Patented accu provides stored kinetic energy to ride through mains interruptions; designed for a 10-year bearing life.

Vibration isolation

Thanks to the solid base frame with isolators between frame and equipment and direct floor installation, vibrations are reduced >97% .

Power panel

A power panel comprising input, output and automatic bypass circuits; additional upstream, down-stream or tie-breakers can be added, if required.

Control system

KS Vision HMI control system; class-leading electrical and mechanical monitoring including load level, mains failures, input and output voltage, frequencies and power factor; data logging feature recording all historic events.

Electromagnetic clutch

The prime starter system consists of standard engine starting motors. The clutch is maintenance-free and guarantees the diesel engine to start at all times, thanks to the redundant start feature.

1

mtu diesel engine

Complying with the latest emissions standards; preheated; quick start and not running during conditioning mode pre-lubricated.

2

Synchronous machine

Four-pole synchronous machines from world-renowned manufacturers designed not to exceed Class F temperature rise; right-sized for your application and to absorb load harmonics.

3

Kinetic energy module

Patented accu provides stored kinetic energy to ride through mains interruptions; designed for a 10-year bearing life.

4

Vibration isolation

Thanks to the solid base frame with isolators between frame and equipment and direct floor installation, vibrations are reduced >97% .

5

Power panel

A power panel comprising input, output and automatic bypass circuits; additional upstream, down-stream or tie-breakers can be added, if required.

6

Control system

KS Vision HMI control system; class-leading electrical and mechanical monitoring including load level, mains failures, input and output voltage, frequencies and power factor; data logging feature recording all historic events.

7

Electromagnetic clutch

The prime starter system consists of standard engine starting motors. The clutch is maintenance-free and guarantees the diesel engine to start at all times, thanks to the redundant start feature.

"A colleague from the night shift recently told me that the whole town was suddenly dark because the power had gone out. Only at Vetter were the lights still on and we were able to continue production." An example that shows how relevant and important the system is.  

50 uses per year for mtu Kinetic PowerPacks

The mtu systems at the various Vetter sites are used around 50 times a year. There is not always a really big power outage that causes the lights to go out in the whole city. The mtu Kinetic PowerPacks also compensate for fluctuations and irregularities in the power grid. And these are occurring more and more frequently - partly because more and more renewable energy is being fed into the grid, making it more volatile.  

When these fluctuations occur, there is a specific trigger logic that has been refined over decades, as Christoph Webinger explains. He has been selling the dynamic UPS systems, which have been part of Rolls-Royce since 2020 and were previously known as EuroDiesel and Kinolt, for 15 years. If there's one expert in this field, it's him.

"If there are only minor fluctuations or phase failures in the power grid, the KPP system remains connected to the grid and merely compensates for the output voltage," says Webinger. At a certain point, however, the diesel engine has to step in and take over the load in order to supply the energy that Vetter needs for its really clean cleanroom.

The mtu Kinetic PowerPacks are regularly serviced. Every two months, a minor inspection is carried out, during which, among other things, the bearings are lubricated and the vibrations are checked.

Nine mtu Kinetic PowerPacks are already in operation at the Ravensburg site, and two more will be added soon. The eleven systems will then have a combined output of 16,000 kilowatts. They are regularly serviced to ensure that they are reliably ready for use at all times. A small inspection is carried out every two months to lubricate the bearings and check the vibrations, among other things. Once a year, the diesel engine also needs to be serviced. "Compared to other uninterruptible power supply systems, however, the maintenance effort for the systems is very low," explains Kai Schumacher. The systems only need a complete overhaul after 20 years.

Then they are completely dismantled and refurbished.Then they will be ready for the next 20 years, during which Vetter employees will be able to fill medicines aseptically.  

STORY Power Generation

Wood, HVO and a touch of Swedish romanticism: How to make data centers sustainable

The EcoDataCenter data centres are among the most sustainable in the world – thanks in part to HVO in the tank of the mtu gensets.

by Lucie Maluck

Read more

STORY Power Generation

Into the champagne powder at high speed

In Colorado, skiers and snowboarders can not only enjoy champagne powder, but also North America's fastest cable car.

by Leslie Dagg, Lucie Maluck

Read more

STORY

Direct current, alternating current, emergency power

There is plenty of electricity in the huge offshore wind farms. Nevertheless, mtu emergency power aggregates are indispensable. Why?

by Lucie Maluck

Read more

STORY Power Generation

Capacity market: A model for the whole world?

UK capacity market ensures security of supply

by Katherine Wooltorton

Read more

Connect with Us

Customer Assistance Center

We are here to take your Sales & Service questions around the clock, 365 days a year.

Read more

Sales & Service Locator

Find your local partner for Sales & Service.

Read more

mtu Stories

Reports and interviews about mtu products and solutions.

Read more