Good kindergarten and wide range of leisure activities
The men in the control center are in a good mood. They say they've been living in Aichal for 30 years. The nicest, most relaxing hobby is to go hunting in the taiga woodlands. And their wives? They like the crosscountry skiing, they say, and collecting berries and mushrooms is also popular. In the taiga, however, you have to protect yourself against the swarms of mosquitoes. The company, Alrosa, does a lot to enrich the lives of Aichal's 13,000 residents. There is a very well equipped kindergarten, an ice rink, a swimming pool, a sports hall and a newly built cultural center where choirs and dance groups rehearse.
Retirement at 50
The workers in the vehicle control center say they are both already pensioners, but still have to work because the pension is just 330 euros. In Russia, men retired at age 60 until 2018. There is a pension bonus for Russians living in the far north. An additional bonus is given to people working below 150 meters in open-cast pits. For mechanics in the Alrosa workshops, this means that they used to be able to retire at the age of 55. The two workers in the control center retired at 45 and 50 respectively because they worked in open-cast mining.
The biggest compensation for living in a wasteland is a good wage. The two tipper drivers Michail and Yefgeni earn 1,800 euros a month. They say they go on holiday once a year to China, Thailand or Montenegro. Many also have apartments in warmer parts of Russia – 'on the mainland' as they say in Aichal with more than a hint of irony. As soon as they retire, and their financial situation permits, most people want to leave Aichal. But there would always be a flow of new, young workers, fleet manager Lapygin assured us: “Good pay attracts people.” Today, 13,000 people live in Aichal. 4,000 of them work in the diamond combine, 1,000 of those in the transport sector alone. The brightly painted prefab buildings in Aichal were not built until the 1980s. Before that, there were only timber houses. And before that, the geologists and construction workers who laid out the town and the open-cast mine lived in tents. Until the 1980s, there were no elaborate medical facilities for childbirths.
Mosquitoes, mud and permafrost
Weather conditions in and around the Arctic Circle are extreme. The ground is frozen for seven months of the year. In summer, the ground thaws up to half a meter deep. Aichal is even more remote in summer than in winter because, traveling by car, you can only get to the airport in Polarnoje and to the city of Mirny, 500 kilometers away, where Alrosa's headquarters are located. People cannot go any further because in summer the roads are
muddy, and Aichal is not connected to the Russian highway network. It is therefore anything but easy to ensure supplies for the town with its three diamond mines and two diamond processing plants.
Spectrometric analysis of engine oil for improved maintenance
The first four 136-ton haul trucks with mtu engines were delivered to Aichal in 2005. “At the time, we sent five people to a coal mine in South Yakutia for training, where mtu engines were in use,” reported chief engineer Andrey Kayukov. At 38, he is one of the younger members of the workforce. The acquisition of an expensive spectometric oil analysis laboratory was a major step forward in engine maintenance, he says. Spectrometric analysis of engine oil is now used to detect metallic particles caused by engine wear. This allows conclusions to be drawn about specific damage to the engine. The chief engineer reports that spectrometric analysis has postponed the general overhaul of the engines by a considerable length of time. A general overhaul of the engine is recommended after 25,000 operating hours. But they now have one mtu engine with 40,000 engine hours, and eleven mtu engines with 33,000 to 38,000 engine hours, which have had only minor repairs, but no general overhaul. Two of the mtu engines obtained in 2005 are still in use. “As soon as we find any metal particles in the engine oil, we have an indication of where the fault could be,” said chief engineer Andrey Kayukov.