Rolls-Royce has been awarded a contract by Polat Enerji, one of Turkey's leading investors in the renewable energy sector, to supply a large-scale battery energy storage system with a capacity of 132 MWh. The mtu QG EnergyPack will be integrated into the Göktepe Wind Power Plant near Yalova in northwestern Turkey and will ensure that electricity from renewable sources can be fed into the grid without interruption. Rolls-Royce hat von Polat Enerji, einem der führenden Investoren der Türkei im Bereich erneuerbare Energien, den Auftrag erhalten, ein Großbatterie-Speichersystem mit einer Kapazität von 132 MWh zu liefern. Das mtu QG EnergyPack soll im Windpark Göktepe Wind Power Plant bei Yalova im Nordwesten der Türkei integriert werden und dafür sorgen, dass Elektrizität aus erneuerbaren Energien ohne Unterbrechung ins Netz eingespeist wird.
PRESS RELEASE Energy Storage

Rolls-Royce wins large-scale mtu battery storage order for wind farm in Turkiye

Posted on January 15, 2025

Images [2 Files, 2 MB]

  • Largest battery storage project in Turkiye with 132 MWh capacity
  • Polat Enerji ensures grid integration of renewable energies with Wind energy-BESS system
  • mtu EnergyPack supports grid stability and profitability

Rolls-Royce has been awarded a contract by Polat Enerji, one of Turkiye's leading investors in the renewable energy sector, to supply a large-scale battery energy storage system with a capacity of 132 MWh. The mtu QG EnergyPack will be integrated into the Göktepe Wind Power Plant near Yalova in northwestern Turkiye and will ensure that electricity from renewable sources can be fed into the grid without interruption.

Polat Enerji Board Member Neşet Özgür Cireli said: “We are happy to sign a new investment that will play an important role in the process of achieving Turkiye’s energy independence and environmental sustainability goals. This cooperation will also be a strong example of adapting world-class technologies to Turkiye’s renewable energy targets. In this sense, we are extremely proud to sign Turkiye’s largest Battery Energy Storage System supply agreement with Rolls-Royce. Our project will not only meet today’s energy needs, but will also shape the energy transformation of the future.”

The plant helps to increase the stability of the Turkish power grid and, thanks to the integration of renewable energies, to reduce CO2 emissions. When the wind is strong and the turbines in the wind farm generate more electricity than the grid can absorb, the surplus energy is stored in the battery systems. This prevents grid congestion at times when a lot of electricity is available. Later, the storage units also supply green electricity to the grid when there is no wind but energy is still needed. The mtu EnergetIQ intelligent control platform helps to ensure that the plant can be operated efficiently and thus profitably.

“With the large-scale battery storage system, we are working with Polat Enerji to help stabilize the grid in Turkiye. Our battery solutions, which are among our strategic focus areas, sustainably and reliably support energy supply worldwide,” said Andreas Görtz, President Sustainable Power Solutions at Rolls-Royce Power Systems.

For 35 years, Rolls-Royce Solutions Turkiye has been providing products and services with its own nationwide service network for all industries in which Rolls-Royce Power Systems operates.

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: