PRESS RELEASE Corporate

ROLLS-ROYCE TO DELIVER GAS GENSETS FOR IMG MIDSTREAM POWER PLANTS IN PENNSYLVANIA

Posted on January 27, 2016

At the end of 2015, the power generation provider IMG Development LLC and Rolls-Royce signed a long-term strategic agreement for the supply of Rolls-Royce medium-speed gensets for a minimum of five plants extending into 2020.

Images [2 Files, 2 MB]

  • Long-term supply agreement and long-term service agreement signed
  • First delivery: six medium speed Bergen gas gensets to supply 40 MW of electric power
  • IMG will feed the generated electricity into the local grid

PITTSBURGH, PA, USA / BERGEN, NORWAY – At the end of 2015, the power generation provider IMG Development LLC and Rolls-Royce signed a long-term strategic agreement for the supply of Rolls-Royce medium-speed gensets for a minimum of five plants extending into 2020. The first part of the agreement involves the delivery of six B35:40 gas generating sets designed for two new power plants in Pennsylvania, USA, that will be operated by affiliates of IMG Midstream LLC. The two companies also signed a long-term service agreement for the systems being supplied to the two plants. The power plants will feed up to 40 MW of electric power into the local grid. Bergen Engines is part of Rolls-Royce Power Systems.

Three gensets, each of which will produce 7,010 kW of electric power, are to be installed in each power plant. The gensets are based on the medium-speed 16-cylinder B35:40 gas engine from Bergen Engines.

Ron J. Kiecana, Senior Managing Director and Board Member at IMG said: “Rolls Royce has the right end-to-end power generation solution to help us rapidly deploy our distributed generation model in infrastructure constrained areas with the type of flexible power needed to address a dynamic energy market where traditional energy supply and consumption patterns are changing. We are excited about this partnership and growing our distributed power generation model with Rolls Royce in the U.S. market.”

Matthias Vogel, Head of Power Generation Business at Rolls-Royce Power Systems, added: “We are delighted with the new long-term cooperation with IMG Development LLC and the trust IMG has placed in our products.”
Helge Skaar Communication Director, Bergen Engines AS
Phone:
+47 55 53 63 18
E-mail:
Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: