CASE STUDY Power Generation

How we protect the environment and DNA samples from around the world

Posted on November 12, 2020

mtu Kinetic PowerPack for world's leading institutes and organizations in genomics and computational biology ensuring uninterruptable power to overcome some of humanity's most significant challenges.
Details

Who

Wellcome Trust Sanger Genome Campus

What

Dynamic UPS

Why

To establish energy saving and reduce carbon emissions

Where

Hinxton, England

Situation

The Wellcome Trust Sanger Genome Campus in Hinxton (England) is home to some of the world's leading institutes in genomics and computational biology, committed to delivering life-changing science with the reach, scale, and imagination to overcome some of humanity's most significant challenges.

Their IT infrastructure is one of the most advanced in the world and contains data research from every corner of the world that must be accessible at all times. The key challenges in this project were retaining the beautiful natural scenery and completion of the scheme with a reduced carbon footprint.

Solution

To achieve the latter, Campus Facilities Management and staff have worked together to establish energy saving and recycling initiatives and like so, strive to reduce carbon emissions. As part of this aim, they have gained ISO 14001 accreditation. As managing energy costs is obviously good practice, businesses try to predict the events and reduce energy consumption during these periods.

But perhaps more importantly, the battery-free smaller footprint solution, now branded as mtu Kinetic PowerPack after Rolls-Royce acquired the former Kinolt S.A., includes the facility to participate in peak shaving schemes, choosing a self-evident one. Although peak shaving is a secondary function and is immediately aborted when the input mains fall out of tolerance, spare capacity in the dynamic UPS output can be utilized to reduce total site demand from the utility supplier.

Result

Two dynamic UPS systems were designed, built, and installed in three months, supervised by Richard Eve, our Technical Manager in the UK. Each dynamic UPS unit, equipped with top-of-the-line engine exhaust silencers and noise control equipment, is housed in a ground floor purpose built acoustic enclosure rated at 65dBA @1m in conditioning mode and 75dBA @1m in the engine running mode.

The controls for each system are housed in a separate switch room enclosure on the first floor, which also contains a close fit 11kV substation with a Schneider ringmaster and ANAN transformer. An underbelly fuel tank located underneath the D-UPS supports the unit for 48 hours of operation of the engine at a 75% load. All of the above is now supported and serviced by our service personnel. The units are remotely monitored, and any incident will be noticed by Rolls-Royce’s unique HMI, KS® VISION.

Looking for Dynamic UPS related sales or service partners?

Power Generation

mtu safeguards continuous emergency operation at Kårstø natural gas processing plant

The Norwegian natural gas processing plant at Kårstø has been equipped with a new emergency power system as part of a long-term expansion project. During any future power outages, five mtu gensets powered by Type 16V 4000 G63 engines will be in place to supply the energy for essential production processes — and, thanks to special acoustic technology, they will do their job more quietly than ever.

Read more

Power Generation

E-vehicle superchargers in Austria more reliable thanks to mtu battery systems

Pull over, fill up, drive on – without losing time. What drivers of petrol-powered automobiles have long taken for granted will, over time, become the new norm for E-drivers too. Many utility grids tend to reach overload when having to cope with several E-vehicles being charged at the same time, or with super-chargers that are demanding high power delivery quickly. Now SYNERG-E, an EU-funded tech project, is helping E-vehicle service stations overcome these challenges at several locations in Austria. How? With stationary battery storage systems carrying the Rolls-Royce brand mtu.

Read more

Power Generation

Sustainable Hybrid System ensures cost-effective power supply in Australia’s Northern Territory

Many aboriginal communities in the Northern Territory of Australia power their homes by electricity generated from diesel power plants. With the aim of reducing the dependence on diesel fuel and acquire the advantages of using renewable energy, Power and Water Corporation started a project located in small community of Daly River. The project expanded the power plant by implementing solar modules and a battery storage unit from the Rolls-Royce solution brand, mtu (former Qinous). The hybrid system project achieved a reliable 24/7 energy operation and currently reduces fuel consumption by 50 percent.