What distinguishes a good engine? Very high injection pressures? Precisely designed and manufactured components? Low-soot combustion? The answer is all of those things – though the really decisive factor is the interaction between them. And controlling and monitoring that interplay is a key engine technology. The engine management system is the brains of the engine that controls key systems such as fuel injection, turbocharging and exhaust gas recirculation. That makes it so important that it is produced in-house at mtu rather than bought in from an outside supplier.
An air-conditioned room, staff in white lab coats and a soft humming sound. Is this what you would imagine an engine factory to look like? It sounds more like a dental surgery. But this large, sterile room is the mtu Electronics Center. Clicking and clacking sounds emanate from a large white robot. With micrometer accuracy, a pick-and-place machine precisely places tiny components weighing hardly five milligrams, such as capacitors, resistors and diodes, on a printed circuit board. Depending on the control unit, a circuit board can have anything from 1,500 to 2,000 components that are placed on the board from large reels and then soldered in position. In that way, a bare green circuit board can be made into a virtually complete printed circuit assembly in just a few minutes. At this stage, however, it is not quite the finished article – it still has to be X-rayed and have ist final few large components fitted by hand. The subsequent visual inspection is also an integral part of the production process. Every single one of the less than pinhead-sized components has to be firmly fixed in the right place. "In the tough conditions that diesel engines are asked to operate in on a daily basis, we have to be able to rely on the control system," explains Heinrich Dageförde, the man in charge of control unit production at mtu.