Red wooden houses, idyllic coastal towns, secluded lakes, cosiness. Anyone who thinks of Sweden has these images in their head. So it fits into the picture that Sweden is home to data centers that are among the most sustainable in the world. Built from wood, of course. With mtu gensets as a backup for the power supply - sustainably powered by HVO.
"We want to lead the way in terms of sustainability," says Mikael Svanfeldt. The 40-year-old is CTO of EcoDataCenter and the brain behind the unique design of the Swedish company's three existing data centers. A fourth is currently being built. The guiding principle for all data centers is the circular economy. This starts with the raw material from which the buildings are constructed: Wood. "Wood is a renewable raw material and therefore more sustainable than steel or concrete, and it also stores CO2 instead of releasing it into the air," explains Svanfeldt. All EcoDataCenter data centers obtain 100 percent of their electricity from renewable sources, mainly from hydropower and wind power, which are available in abundance in Sweden. And the waste heat generated by the servers is reused in the nearby biofuel production plant.
With these measures, Mikael Svanfeldt and his team have managed to reduce the PUE value of the data centers to 1.15, withput any compromize to the quality of services delivered. This value puts the total energy consumption of a data center in relation to the energy used purely for the IT equipment. "We are proud of the 1.15, because that puts us at the lowest limit," says Svanfeldt.