And what were the results?
We already know that for every 1,000 litres of diesel burned, we’re producing approximately 3.6 tonnes of greenhouse gas CO2, compared to just 195kg greenhouse gas CO2 for every 1,000 litres of HVO burned. Simply by switching diesel for HVO, our clients are reducing their net CO2 greenhouse gas emissions by up to 90% right away - well to tank.
But what does that equate to real terms? If a 60MVA site had to run continuously at 100% load for a period of 36 hours due to the lack of availability of grid power (let’s face it, this is what standby generators are designed to do), then the total fuel consumption across the backup generator engines would be approximately 15,225l of diesel per hour. That’s a lot of diesel burned, and a lot of CO2 produced keeping the power running and supporting the critical infrastructure. When we look at the parameters of the site involved running on HVO as opposed to diesel, the switch would mean a saving of 1.86 million tonnes of CO2 over the course of the shutdown. That’s the equivalent of taking 1000 average size family diesel cars off the road for a whole year.
But the reductions in CO2 are just one element to consider.
Exactly. But we also compared the particulate matter (PM), nitrogen oxide (NOx) and hydrocarbons (HC) emissions of HVO in comparison to standard diesel – all of which produced some significant savings and created an immediate improvement in local air quality. Using the same example site as earlier, running on HVO as per the 36-hour shutdown above, the particulate matter savings would be around 51.101 kg (>30%).
Putting this into context based on a standard diesel car, the savings from running on HVO would be similar to 1000 diesel cars travelling 11,300km (Dublin to Hanoi, Vietnam). This would cover 3.5 full sized football fields with a visible black dust. The NOX saving from switching to HVO (>20%) would be equivalent to a diesel car travelling 34,837km (Dublin to Ankara, Turkey). As for the Hydrocarbon savings, that would be the same as a 1000 diesel cars driving to Andorra (1,300Km).