STORY Commercial Marine

Ship of the year sails with mtu

Posted on March 11, 2024 by Lucie Maluck, Images by Signet Maritime

Thanks to their unparalleled maneuverability and low emissions, two mtu-powered American tugs have won the "Workboat of the Year" award.
mtu tugboat engines
Uncompromisingly reliable mtu propulsion systems provide maximum maneuverability and a strong bollard pull for your workboat at all times.
Read more
Signet Sirius and Signet Capella are the ships of the year 2023 in the USA. The international trade magazine "Work Boat" awarded this prize to the two tugs of the Signet Maritime shipyard. Each tug is powered by three mtu Series 4000 engines that were sold through the Rolls-Royce Power Systems Partner, Pacific Power Group (PPG).


Signet Sirius  and Signet Capella  are not only incredibly strong with a bollard pull of 92 tons, they are also the first vessels in the USA to receive an ABS ENVIRO and an ABS LEV (Low Emission Vessel) label. To achieve this, the Particulate Material (PM) emissions from the engines must be significantly below the Tier 4 commercial marine limits set by the US Environmental Protection Agency (EPA) -- the latest generation of mtu Series 4000 engines do just that. Each of the 12-cylinder engines has a power output of 2575 bHP (1,920 kW) and benefits from over 25 years of evolution resulting in drastic improvements in the time between overhaul (TBO).  

"Signet Sirius" and "Signet Capella" are powered by three Tier 4 mtu Series 12V4000 M65L engines.

Rotortugs guarantee excellent maneuverability

The tugs have three drive systems installed in each tug: two in the bow and one in the stern. This typical rotortug design gives the two tugs, which were designed by renowned tug designer Robert Allen, unparalleled maneuverability and enormous stability on the water.  

Use in challenging waters

The Signet Sirius is already in service, escorting large oil tankers,  known as VLCCs, through the Texas Aransas Passage to Ingleside, the largest crude oil storage and export terminal in the United States. With its strong currents and comparatively high waves, the passage is particularly challenging for ships. "The stability in performance during a bollard pull with full engine power and pitch to the propellers, the vessel squats down in the water and stays uncharacteristically stable with little side-to-side movement. The engine metrics between the three are extremely tight providing consistent “continuous rated power” that we only get from Rolls-Royce & PPG," says Tim McCallum.  

Made for the toughest conditions: The "Signet Sirius" is already underway in the Texas Aransasa Passage, which is known for strong currents and high waves.

Christof von Bank, responsible for the Rolls-Royce marine business in the USA, was delighted with the award for the mtu-powered tugs: "We are very pleased with the results of this particular project, the performance of the mtu engine and SCR system has exceeded our expectations. It shows that we have one of the most powerful solutions on the market and we are confident that we will see more Series 4000 M05 engines in the tug market in the near future."

STORY

Direct current, alternating current, emergency power

There is plenty of electricity in the huge offshore wind farms. Nevertheless, mtu emergency power aggregates are indispensable. Why?

by Lucie Maluck

Read more

STORY Commercial Marine

Special missions of a service nomad

It took just 4 ½ weeks for Melik Meddur and his team to perform a major overhaul of the three Series 8000 units powering the ferry HSC Condor Liberation, operated by British operator Condor Ferries. They did the job with the engines in-situ, i.e. in the engine room itself. Quite a feat, but by no means a premiere for Melik. So what's life like for him as a Rolls-Royce 'service nomad'?

by Lucie Maluck

Read more

STORY Commercial Marine

"The gas engines purr quietly like kittens"

It has something of a premiere atmosphere: Europe's first inland ferry powered by a high-speed pure gas engine is about to go into operation on Lake Constance. It is still being diligently tested.

by Lucie Maluck

Read more

STORY Commercial Marine

Halunder Jet now safer and more efficient – thanks to NautIQ

The mtu NautIQ Foresight equipment health management system is ensuring the Halunder Jet catamaran can shuttle back and forth between Hamburg and Heligoland with maximum uptime and minimum fuel consumption.

by Lucie Maluck, Anne-Katrin Wehrmann

Read more

Connect with Us

Customer Assistance Center

We are here to take your Sales & Service questions around the clock, 365 days a year.

Read more

Sales & Service Locator

Find your local partner for Sales & Service.

Read more

mtu Stories

Reports and interviews about mtu products and solutions.

Read more