Cannes.jpg
PRESS RELEASE Yacht

From bridge to propeller: Rolls-Royce expands mtu propulsion portfolio for yachts

Posted on September 08, 2026

Images [3 Files, 1 MB]

  • Variable-speed mtu Series 2000 gensets enable efficient propulsion and power supply on board
  • New exhaust after-treatment system for mtu Series 2000 engines for yacht operation in emission-regulated sea areas

Rolls-Royce is further expanding its portfolio for yachts and introducing two systems based on the mtu engine Series 2000: standardised variable-speed gensets and a new SCR exhaust after-treatment system. The propulsion system is so compact that it enables the single-deck engine room concept, which is highly advantageous for yachts. With these new solutions, Rolls-Royce is strengthening its holistic ‘From Bridge to Propeller’ approach, in which propulsion, energy management and automation work in tandem.

“Our aim is to offer shipyards and owners a comprehensive and future-proof range of solutions for yachts. This is not just about individual components, but about the optimal interaction of the systems on board to deliver greater performance, efficiency and lower emissions,” said Dr Lukas Köhler, Senior Vice President Global Marine & Mining at Rolls-Royce Power Systems.

A key component of this expanded range is the standardised variable-speed gensets based on the mtu Series 2000. They adjust their engine speed to the actual power demand, thereby reducing fuel consumption and CO₂ emissions during operation by up to 15 per cent. At the same time, they operate around 6 dB more quietly, which significantly improves comfort on board.

With electrical outputs ranging from 650 to 1,850 kWe, the gensets cover a broad power range. Their high-power density and compact design allow for flexible integration even where installation space is limited. They are also suitable for battery-assisted marine applications and can be used, for example, as range extenders.

The product is based on Rolls-Royce’s decades of experience with diesel-electric propulsion systems. Numerous large vessels already have variable-speed mtu gensets based on the Series 4000 on board, and many yachts benefit from diesel-electric propulsion systems based on the Series 2000.  

The new SCR exhaust gas after-treatment system also expands the range of applications for the mtu Series 2000 in emission-regulated sea areas. The system, which is being certified in collaboration with exhaust gas after-treatment specialist Eminox, meets the requirements of IMO Tier III and reduces nitrogen oxide emissions by 75 per cent compared with the IMO II limits. Depending on the load profile, the solution is designed for a service life of up to 16,000 operating hours, requires no compressed air for dosing and can be flexibly integrated into a variety of vessel designs.

With ‘From Bridge to Propeller’, Rolls-Royce aims to view the yacht as a complete system: from the controls on the bridge to the propulsion in the water. To this end, the company combines its expertise in propulsion systems, energy management and automation to create integrated solutions that improve efficiency, safety and cost-effectiveness.

For shipyards, this approach offers an additional advantage: they receive a coordinated solution from a single source. This reduces the effort involved in design and integration, whilst minimising interface risks. The interlinking of mtu propulsion systems, mtu NautIQ Bridge and automation technologies creates a unified digital environment. It helps shipyards and owners to manage energy flows, reduce emissions and increase operational uptime – a step towards a more modern and comfortable yachting experience. 

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: