PRESS RELEASE Commercial Marine

Rolls-Royce powers world’s fastest offshore crew transfer vessels

Posted on January 27, 2025

Images [4 Files, 4 MB]

  • Sea trials demonstrate maximum speed exceeding 53 knots under operational load
  • Each of the three ships is powered by four 16-cylinder mtu Series 2000 engines
  • 35-meter ships are designed as “Surface Effect Ships” (SES)

The Singapore shipbuilder Strategic Marine has commissioned a series of three new offshore supply vessels with a maximum speed of over 53 knots - the fastest of their kind in the world. Each vessel is powered by four 16-cylinder mtu Series 2000M72 engines from Rolls-Royce. The vessels will be used by a national oil company in Africa for passenger transfer to offshore platforms and Floating Production, Storage and Offloading vessels.

To enable fast and safe passenger transfer to offshore platforms, the 35-meter-long vessels have been designed as so-called “Surface Effect Ships” (SES). SES uses air-cushion technology within a catamaran hull form. This design was used for the first time in the offshore oil and gas industry.

The boats have an optimized power-to-weight ratio and use powerful fans to generate an air cushion between the hulls that minimizes hull drag and resistance. Combined with the mtu propulsion package (each delivering 5,760 kW of power), the vessels can travel at much higher speeds than conventional monohulls and catamarans, with consumption remaining at the same per hour of operations. The high speed of well over 50 knots (more than 90 km/h) ensures shorter transit times, while the low hull resistance saves fuel and reduces emissions.

“Our goal in building these crew transport vessels was to minimize the water resistance at the hulls and maximise the cruising and top speed of the ship. The 53-knot top speed during the sea trials demonstrates that we were successful in building and commercialising this technology for offshore crew transfer applications. mtu engines have made a significant contribution thanks to their unique power-to-weight ratio,” explained Chan Eng Yew, CEO from Strategic Marine.

“We are extremely proud that our mtu propulsion package has helped to develop this new and extraordinary type of vessel,” said Denise Kurtulus, Senior Vice President Global Marine at Rolls-Royce Power Systems. “The excellent power-to-weight ratio and long maintenance intervals of over 12,000 hours were crucial factors in the selection of our engines. These product benefits will help us achieve our strategic goal of increasing our share of the commercial marine market.”

This video shows how a surface effect vessel works: AIRCAT 35 Crewliner

About Rolls-Royce Holdings plc

  1. Rolls-Royce develops and delivers complex power and propulsion solutions for safety-critical applications in the air, at sea and on land. Our products and service packages enable our customers to connect people, societies, cultures and economies together; they meet the growing need for power generation across multiple industries; and enable governments to equip their armed forces with the power to protect.
  2. Rolls-Royce has a presence in 48 countries and customers in more than 150, comprising over 250 commercial large aero engine customers, 160 armed forces and navies and approximately 40,000 active Power Systems customers. We are committed to becoming a net zero company by 2050 and we support our customers to do the same.
  3. Annual underlying revenue was £15.4bn in 2023, underlying operating profit was £1.6bn and free cash flow £1.3bn.  
  4. Rolls-Royce Holdings plc is publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  5. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,500 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: