The first 20-cylinder mtu Series 8000 engines to power the three new Miecznik-class frigates for the Polish Navy are currently being built at the Friedrichshafen plant of the Rolls-Royce Power Systems division.Die ersten 20-Zylinder-Motoren der mtu-Baureihe 8000  für den Antrieb der drei neuen Fregatten der Miecznik-Klasse für die polnische Marine entstehen derzeit im Friedrichshafen Werk der Rolls-Royce-Division Power Systems.
PRESS RELEASE

Rolls-Royce supplies mtu propulsion and on-board power systems for three new Polish Navy frigates

Posted on May 29, 2024

Images [2 Files, 7 MB]

  • Twelve 20-cylinder mtu Series 8000 engines for Miecznik-class ships
  • On-board power supply for multi-purpose vessels with twelve mtu Series 4000 marine gensets

The mtu propulsion engines and four marine gensets for the propulsion and power supply of the first of three new Miecznik multipurpose frigates for the Polish Navy are currently being built at Rolls-Royce in Friedrichshafen, Germany. Four mtu 20V8000 main propulsion engines with 8,200 kW each and four mtu 12V4000 on-board generators with 1650 kW mechanical power each will be installed on each ship.

The four main propulsion engines of the CODAD propulsion system, two per propeller, can be used flexibly in different combinations - from single engine operation for slow patrols to high-speed operation at over 20 knots (37 km/h) with all four engines. At a cruising speed of 12 knots (approx. 22 km/h), the Miecznik-class ships have a range of around 8,000 nautical miles (almost 15,000 kilometers).

The four mtu on-board power generators feed the electrical power grid for ship and mission operations independently of the propulsion engines. The frigates are equipped with weapon and mission systems to monitor and control sea areas, protect naval bases and attack surface, underwater, land and air targets.

The first ship of the Miecznik (swordfish) class, which is based on the British Arrowhead 140 concept, is currently being built at the state-owned PGZ shipyard in Gdynia. The first ship is scheduled to be launched in 2026 and commissioned in 2030, with the other two ships to be handed over to the Polish Navy by 2031.

“This order as part of our strategic initiative in the government business not only further consolidates our strong position in the market for propulsion systems for very fast ships. With these state-of-the-art systems, we are also supporting our NATO partner Poland, with whom we have a long-standing partnership,” says Paul Röck, Defence Sales Director for EMEA and Latin America at Rolls-Royce Power Systems.

Since its launch in 2000, the mtu Series 8000 has become the benchmark for high-speed high-performance diesel engines. The 20-cylinder variants with an output of up to 10,000 kW are used worldwide in naval and government vessels as well as in commercial fast ferries with top speeds of over 38 knots (70 km/h). They are characterised in particular by high acceleration, economical operation and ease of maintenance. A variant of the 8000 with 16 cylinders and up to 8000 kW is now also in the programme. "The wide performance range of the 8000 series, from unlimited low-load operation to rapid deployment, is of particular interest to government and armed forces vessels," emphasises Paul Röck.

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Wolfgang Boller Spokesman Regional and Business Media
Phone:
+49 7541 90 2159
E-mail: