Tadano opts for mtu engines from Rolls-Royce for its all-terrain cranes
Posted on March 22, 2022
- Sealing of long-term partnership in German-built Tadano cranes
- Majority of Tadano all-terrain cranes produced in Germany to be powered by mtu engines from Rolls-Royce
Crane manufacturer Tadano is harmonizing the crane portfolios of its German subsidiaries Tadano Faun and Tadano Demag and in the future will be relying more strongly on mtu engines from Rolls-Royce. The move signifies a deepening of the already long-standing cooperation between the two companies. Cranes built in Lauf an der Pegnitz and Zweibrücken in Germany are sold in many countries worldwide.
Most of Tadano’s 26 crane models with two to nine axes and payloads from 45 to 700 tons are already powered by in-line mtu Series 1000, 1100, 1300 and 1500 engines. These deliver power outputs from 129 to 480 kW, and besides compliance with EU Stage III to V emissions standards boast impressively low running costs, high reliability and an excellent power-to-weight ratio. Expansion of the partnership will see the sale of around 3000 mtu engines and Daimler transmissions by the end of 2025.
High-torque mtu engines already power all of Tadano’s crawler cranes – a segment in which Tadano, with payloads of up to 3,200 tons, is at the forefront of the world market – and shall continue to do so.
Jens Ennen, President and CEO of Tadano said: “This cooperation agreement marks a milestone in the re-orientation of our mobile crane business. We’re delighted to have strong, reliable partners like Rolls-Royce and Daimler Truck at our side as we grow. Even in the midst of the pandemic with its supply chain uncertainties, Rolls-Royce has continued to deliver reliable drive solutions of the highest quality.”
Dr Lei Berners-Wu, Vice President Global Industrial at Rolls-Royce business unit Power Systems, said: “This agreement deepens the cooperation between two companies who are already an excellent fit. Tadano and Rolls-Royce both look back on a strong tradition and are using their innovative products to tackle the future jointly.”
Rolls-Royce business unit Power Systems is currently undergoing a transformation from engine manufacturer to provider of sustainable, integrated drive and power generation solutions. With its sustainability program ‘Net Zero at Power Systems’, it is moving decisively towards its goal of climate-neutral solutions. Hence most of the engines supplied to Tadano are certified for use with sustainable fuels and can therefore be run to achieve a net-zero emissions balance. “We’re already swapping ideas with our partner Tadano on other climate-neutral technologies,” said Berners-Wu.
Tadano’s standard platform strategy, of which mtu engines form an integral part, reduces the complexity of its portfolio, enabling customers worldwide to benefit from even better products and a more streamlined service. Besides engines, transmissions from Daimler Truck AG are also incorporated into the new platform strategy.
About Rolls-Royce Holdings plc
- Rolls-Royce pioneers the power that matters to connect, power and protect society. We have pledged to achieve net zero greenhouse gas emissions in our operations by 2030 (excluding product testing) and joined the UN Race to Zero campaign in 2020, affirming our ambition to play a fundamental role in enabling the sectors in which we operate achieve net zero carbon by 2050.
- Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 9,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids and is intensively engaged in the development of climate-neutral solutions.
- Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces and navies, and more than 5,000 power and nuclear customers.
- Annual underlying revenue was £10.95 billion in 2021, underlying operating profit was £414m and we invested £1.18 billion on research and development. We also support a global network of 28 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.
- Rolls-Royce Holdings plc is a publicly traded company (LSE:RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
Contacts
Phone: |
+49 7541 90 3461
|
E-mail: |