Indian Coast Guard places trust in mtu engines from Tognum
Posted on September 10, 2009
The Engines Division of propulsion and power specialist Tognum has received two orders for the supply of mtu engines and automation systems for 23 new ships for the Indian Coast Guard.
- mtu Series 2000 and 4000 engines to be main propulsion units for new Indian Coast Guard craft
- Specifications include mtu Callosum and Blueline automation systems for propulsion control and ship monitoring
- Tognum subsidiary MTU Asia secures contract worth 32.5 million euro
Friedrichshafen/Singapore, 10 September 2009. The Engines Division of propulsion and power specialist Tognum has received two orders for the supply of mtu engines and automation systems for 23 new ships for the Indian Coast Guard. The total value of the contracts is 32.5 million euro. The engines are to be delivered between the end of 2009 and the end of 2011.
“These contracts secured by MTU Asia demonstrate once again that business in the government vessels sector is a very steady, strong and essential component of our overall portfolio. It is also especially important in economically difficult times“, states Rainer Breidenbach, Tognum COO with responsibility for the Engines Division.
Eight new Inshore Patrol Vessels are to be powered by triple Type 16V 4000 M90 engines with an output of 2,720 kW (3,648 bhp) each. In combination with waterjets, they will propel the vessel at speeds up to 35 knots. The systems to be supplied for the 48-meter patrol vessels include the mtu Callosum ship automation system with an integrated solution for monitoring all ship’s services that also incorporates fire detection and extinguishing systems. The reliable, easy-to-maintain and low fuel consumption engines enable the patrol vessels to remain at sea for a prolong period of time without having to return to base to replenish supplies.
The Tognum Group is also supplying 30 mtu Type 16V 2000 M92 engines each capable of 1,630 kW (2,186 bhp) for 15 Interceptor Boats in the 26-meter class. They will provide the boat with a top speed of 35 knots. Engine control and system monitoring will be performed by the mtu Blueline automation system.
The Series 4000 engines will be delivered as assembly kits to the licensed producer in India, Garden Reach Shipbuilders and Engineers (GRSE) in Kolkata, for local assembly and testing. Meanwhile, the Series 2000 units will be sent to the Bharati shipyard in Mumbai.
The construction of the new ships is part of an expansion of the Indian Coast Guard. The varied duties of the Indian Coast Guard are fishery protection, combating smuggling and terrorism, prevention of illegal immigration, search and rescue operations as well as marine environment protection.
Tognum subsidiary MTU Asia has already sold more than 100 Type 16V 4000 M90 engines to the Indian Coast Guard and Navy in recent years. They are highly valued for their proven reliability, outstanding power-to-weight ratio and also the well-established mtu service network in India.
Phone: |
+49 7541 90 2159
|
E-mail: |