Reman plants of Rolls-Royce in Germany and North America
The heart of Rolls-Royce's remanufacturing processes is located in Magdeburg - in addition to a recently expanded plant in North America. In the reman plant, complete mtu engines and systems as well as individual components are reconditioned and reused using standardized processes. More than 40,000 products have already undergone the Reman process there. Between 150 and 250 rail PowerPacks, for example, arrive in Magdeburg every year and leave the plant in as-new condition - ready for another 18,000 hours of operation.
Reman: Industrial refurbishment in a standardized process
The term "reman" (from remanufacturing) refers to the industrial refurbishment of main components and motors. In standardized processes, the systems and engines are first disassembled into their individual parts, cleaned and tested for function and wear. The individual parts are then refurbished, assembled, painted and reassembled with Reman components or new parts. The engines that are reconditioned at the Reman plant in Magdeburg are then as good as new. The high quality is guaranteed by automatic improvements to the engine and strict functional tests, which are subject to the same criteria as for new engines. Therefore, the same warranty conditions apply to a Reman engine as to a new engine.
Attractive for customers: Remanufacturing within 15 days
To keep train downtimes as short as possible for customers, the Magdeburg site has set itself up in such a way that products can be overhauled within a maximum of 15 days. For some Series, Rolls-Royce can also provide replacement PowerPacks or engines, so-called "swing units", before the drive unit is removed. Customers can install these "replacement engines" in their railcars or locomotives and do not have to wait until the first systems have gone through the remanufacturing process. "In this way, we keep downtimes to a minimum for our customers," explains Marc Goldschmidt.
Rolls-Royce has also established a deposit system to help boost recycling. This creates financial incentives for the return of used engines by giving customers a credit note, the amount of which depends on the condition of the returned engine.
Netinera has also been relying on Rolls-Royce reman solutions for many years. The company is one of Germany's largest transportation companies and operates local and regional public transport services with buses and trains. Rolls-Royce has already overhauled and remanufactured numerous mtu engines and mtu rail PowerPacks on behalf of Netinera in the past.