Die Coradia Lint 54-Züge bieten mehr Platz und Komfort, sind gleichzeitig leiser, effizienter und stoßen deutlich weniger CO2 und Partikel aus als die bisher eingesetzten Züge.
STORY Rail

Regional trains by Lake Constance with mtu power

Posted on September 23, 2019, Images by Robert Hack, mtu

The Coradia Lint 54 offer more space and comfort, are quieter, more efficient, and emit significantly less CO2 and particles than the trains used hitherto.
Friedrichshafen, Germany

There is good news for passengers, local residents and the environment in southern Germany’s Lake Constance area, the traditional home of mtu: Five new trains have recently taken to the tracks there, fitted with mtu traction systems. The Coradia Lint 54 regional trains from Alstom offer more space and comfort, are quieter, more efficient, and emit significantly less CO2 and particles than the trains used hitherto. The vehicles owe the latter to their three modern mtu PowerPacks, each equipped with a Series 1800 engine that meets the stringent EU Stage IIIB emission requirements. The drive systems can accelerate the trains between Friedrichshafen and Radolfzell to speeds of up to 140 kph.  

Rolls-Royce customer Alstom delivered the new Coradia Lint trains on schedule to local operator Südwestdeutsche Verkehrs-Aktiengesellschaft (SWEG), which operates them on behalf of DB Regio Alb-Bodensee (RAB). The Coradia Lint trains are now used daily in regional transport services on the shores of Lake Constance. 

The use of Coradia Lint trains could also be an important step on the way towards the use of hybrid rail drives on the Lake Constance Belt Railway: Rolls-Royce is currently cooperating with vehicle manufacturer Alstom to investigate the economic feasibility of repowering these trains with mtu Hybrid PowerPacks. Winfried Hermann, Minister of Transport in the state of Baden-Württemberg, commissioned this study last May during a visit to Rolls-Royce Power Systems. He was impressed by the environmentally friendly hybrid traction system from Friedrichshafen: “I am excited about the mtu Hybrid-PowerPack: it is a promising innovation which has been developed in our home state of Baden-Württemberg. We would like to test it here as well.” This vision is now one step closer. 

The content of the stories reflects the status as of the respective date of publication. They are not updated. Further developments are therefore not taken into account.

Point of contact

Michael Miltz
Phone:
+49 7541 90 3846
E-mail:

Related stories

Rail

"We could already be saving 90% of CO₂ today – but we prefer to discuss it."

A conversation with Dr. Olaf Toedter (Head of New Technologies and Ignition Systems at the Karlsruhe Institute of Technology) and Jörg Schneider (Head of Sustainability at DB Cargo) about HVO, eFuels, and the technologies that no one can see yet.

Read more

Rail

Cruise Train on rails

Superlative in every respect, the Train Suite Shiki-Shima is powered by electricity generated by two mtu Series 4000 engines on non-electrified routes.

Read more

Rail

mtu Power for Heavy-duty Steelworks Locomotives

As many as 28 locomotives are available for operation at the voestalpine Steel Division plant in Linz. Four of them are Gmeinder type D60 C marshaling locomotives each driven by an mtu Series 1600 engine. The locomotives operate on company premises hauling trains that can weigh up to 3,000 tonnes each. Two more units of the same type are on order with delivery scheduled by the end of 2015. The locomotives are operated by logistics company LogServ, a wholly-owned subsidiary of voestalpine Stahl GmbH.

Read more