Today Cannes, in a few days Monaco and in October Fort Lauderdale – yacht lovers from all over the world have descended on the Côte d'Azur or Florida, backdrop for the Cannes Yachting Festival, Monaco Yacht Show and Fort Lauderdale Boat Show, where the yachts displayed are of such breathtaking luxury that a jacuzzi won't even get a mention because it's long since considered a basic.
But it's not only the yachts' graceful forms and their grand furnishings that fascinate. Below deck, there's the technology – the engines, propellers and bridges – all at the top end of the performance spectrum. If they are to function really efficiently, however, they have to be perfectly harmonized. Which is why Rolls-Royce provides all the systems needed to power a yacht – from the bridge to the propeller. That includes fully integrated bridge and automation systems, engines, and highly efficient Pod propulsion. And because all these systems interplay perfectly, maximum efficiency is assured.
Click on the image to find out more: