mtu Series 4000 natural gas generator sets at this distributed energy site provide power to the Alberta grid during times of peak demand that is both reliable and more environmentally friendly than other sources of generation (such as coal and diesel).
PRESS RELEASE Power Generation

Rolls-Royce supplies mtu gas generator sets for large distributed energy project in Canada

Posted on November 07, 2024

Images [1 Files, 1 MB]

  • Internal combustion engines powered by natural gas provide reliable, low-emissions power for energy transition
  • mtu Series 4000 gas gensets support Alberta’s grid during times of peak demand to ensure continuous availability

Rolls-Royce is supplying 10 mtu 20V 4000 L64 FNER gas gensets to its distributor partner Collicutt Energy Services for end user installations in Alberta, Canada. Each site will provide electricity into the grid at times of peak demand ensuring constant availability for the community and industry. The first of the five sites is now online.

The electricity market in Alberta is unique in Canada as it is a for-profit deregulated “energy-only” system that pays power producers for the power they dispatch onto the grid. The wholesale price of electricity is set each hour, and each producer is paid based on the rate at the time of supply, regardless of how that power is produced.

With the mtu Series 4000 natural gas gensets at each site, the power supplied to the grid is both more environmentally friendly and cost-effective than energy produced from other sources such as coal or diesel.

Tobias Ostermaier, President of Stationary Power Solutions, Rolls-Royce, said: “The mtu Series 4000 natural gas gensets are a perfect fit to capitalize on the unique electricity market in Alberta. The high efficiency of the units along with their low emissions make our solution both economically and environmentally attractive.”

Rolls-Royce’s mtu gas gensets were selected for the project based on the related cost of power generation and their long lifespan – offering 84,000 operating hours before major overhaul. Key to the end user’s purchase decision was also the local service support provided by Collicutt Energy Services, Rolls-Royce’s sales and service partner for mtu products in Alberta. Collicutt will provide long term maintenance for the gensets and balance of plant, including 24/7 monitoring at each of the sites.

Producing fewer air pollutants and CO2 emissions than other energy sources, natural gas-fuelled gensets are a bridging technology toward a zero carbon future. Offering clean power alongside high efficiency and maximum performance, the units are also future ready, offering the ability to run on both natural gas and hydrogen blending.

As the project lead, Collicutt oversaw every phase, from the initial concept through the engineering, design, manufacturing, assisting with the onsite installation, and final commissioning. The project’s design focused on a sophisticated plug-and-play system, significantly reducing onsite construction time and streamlining commissioning. Throughout the process, Collicutt also prioritized minimizing environmental impact and overall waste while enhancing project efficiency.

“As renewable energy sources like solar and wind continue to expand, the stability of the power grid can fluctuate when the sun isn't shining or the wind isn't blowing. Fast-acting power generation is critical to maintaining grid stability,” said Ryan Krutzfeldt, VP of Operations at Collicutt Energy Services. “That’s where the mtu Series 4000 gas generator comes in. This innovative technology highlights Alberta’s abundant natural resources and skilled workforce, driving the delivery of clean and reliable energy to the market.  Projects like these showcase Alberta's capability to lead in sustainable energy solutions.”

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Jennifer Riley Spokeswoman North and Latin America
Phone:
+1 248 560 8488
E-mail: