Handling
DEF is a non-hazardous, easy-to-use operating fluid. It is not a fuel, nor a fuel additive, but a high purity urea solution that must be stored within a dedicated DEF tank (separate to the diesel tank), that is refilled as/when required. In most cases, the DEF tank and fuel tank are sized proportionally, and will empty at about the same rate. To maintain a proper supply, operators should refill the DEF tank every time they refuel.
A 32.5% urea concentration must be maintained in the DEF solution for optimal operation of the emissions control system. SCR reduces levels of NOX using ammonia as a reductant within the catalyst system. If the concentration is lower, less ammonia is produced. Precise controls for the injection of DEF for the SCR system must be in place to automatically inject DEF to get the proper NOX reduction, while controlling NH3 slip.
The best solutions to maintain optimal DEF concentration are closed loop control systems that continuously monitor inlet and outlet NOX emissions. Most injection control systems can handle minor concentration fluctuations. If an operator notices the concentration of the urea is out of spec and needs to be adjusted, consult with your DEF supplier on the best method for your site to correct this issue. Below are several general guidelines.
If the urea concentration is 40-50%, it is best to add deionized water to the tank in increments of 10% of the volume of DEF in the tank, until it is within specification. Do not use tap water. If the DEF concentration is above 50% (generally crystalized urea is present in the tank), it is best to clean out the DEF system and begin with fresh DEF.
Use heated lines and a heated tank to keep the DEF above the freeze point during the winter months. Often the DEF tank is insulated to lower the heating requirements for the tank. It is ideal to use a vacuum/pressure vent that opens and closes when there is a change in pressure. This will limit evaporation of the water in the DEF and help keep the concentration constant over time.
Always store DEF in High Density Polyethylene (HDPE) or stainless-steel tanks. Since DEF reacts with copper, make sure even connections use the appropriate materials like stainless steel. If copper is used on a connection it can easily be seen, as the DEF will change to a blue color quickly. DEF may seep through connections. If DEF dries and forms crystals, simply use warm water and a rag to remove.