Hydrogen key to CO2-free container logistics
The list of applications in the Duisburg terminal to be powered by electricity generated with hydrogen is long, and ranges from the feeding of vessels with shore power to the unloading, storage and handling of containers. To keep these processes as lean as possible, the port has opted to dispense with conventional vehicles for moving containers within the terminal. Instead, electrical bridge systems will be used to unload the standardized metal containers and place them into storage or onto freight trains and trucks. What makes this project really exciting for Rolls-Royce Power Systems is the fact that the power plant can grow along with the port. Should Duisport be expanded, the mtu energy systems can be expanded alongside it, and with a swiftness that would not be possible with standard main grid connections. The infrastructures for supplying the terminal with hydrogen are expandable too: Initially the fuel will be delivered in cylinders by road, with the addition of rail tank cars and ship tankers at a later stage. Duisport's mid-term plan, however, is to use solely 'green hydrogen' that it receives by pipeline. Ideally, this will have been produced in the region using electrolysis, with the integration of renewable energies such as wind and solar. And Duisport wants to do even more than just use eco-friendly hydrogen. Ultimately, its goal is to become a distribution hub for hydrogen as a future energy source.
Beacon project for ports around the globe
For Rolls-Royce Power Systems, the Duisburg project is an example for other ports, and not just inland ports, to follow: “The integrated applications set up in the port of Duisburg can be implemented just as well in maritime container ports and cruise ship terminals,” explained Fürderer. The demand, he insisted, is there. But while many ports are interested in increasing their capabilities, the capacity of the electrical power grid is not that easy to scale up.