Swedish data center operator Eco Data Center has switched the fuel for its mtu emergency power generators from fossil diesel to sustainable Hydrotreated vegetable Oil (HVO), taking it one step closer to its goal of becoming the leading Nordic provider of sustainable and secure data center solutions. Eco Data Center has gradually expanded at its first major location in Falun, Sweden, and since 2017 has relied on mtu gensets from Rolls-Royce’s Power Systems division for its emergency power supply. Der schwedische Rechenzentrumsbetreiber Eco Data Center hat den Kraftstoff für seine mtu-Notstromaggregate von fossilem Diesel auf das nachhaltige HVO (Hydrotreated Vegetable Oil) umgestellt und ist so seinem Ziel, der führende nordische Anbieter von nachhaltigen und sicheren Lösungen für Rechenzentren zu werden, noch einen Schritt näher gekommen. Eco Data Center hat an seinem ersten großen Standort in Falun (Schweden) nach und nach expandiert und setzt seit 2017 bei der Notstromversorgung auf mtu-Aggregate der Division Power Systems von Rolls-Royce.
PRESS RELEASE Power Generation

Sustainable data protection: EcoDataCenter in Sweden relies on mtu backup generators from Rolls-Royce that run on HVO fuel

Posted on November 14, 2024

Images [3 Files, 3 MB]

  • 32 mtu gensets at EcoDataCenter in Falun ensure uninterrupted power supply
  • Using HVO (Neste MY Renewable Diesel), CO2 emissions are reduced by up to 95%
  • Sustainability is the name of the game: EcoDataCenter provides recovered waste heat
  • EcoDataCenter has relied on Rolls-Royce since 2017 and continues to expand with mtu products

Swedish data center operator EcoDataCenter has switched the fuel for its mtu emergency power generators from fossil diesel to sustainable Hydrotreated Vegetable Oil (HVO), solidifying the ambition of being the leading Nordic provider of sustainable and secure data center solutions. EcoDataCenter has gradually expanded at its first major location in Falun, Sweden, and since 2017 has relied on mtu gensets from Rolls-Royce’s Power Systems division for its emergency power supply. 32 mtu systems based on Series 4000 engines are already ensuring that data from the data center’s customers is backed up even in the case of an outage from the public grid. The next 16 gensets have already been ordered for further expansion. BOS Power, as a local partner and solution provider for mtu products in Scandinavia, is significantly involved.

A commitment to sustainability
EcoDataCenter is committed to building and operating data centers that are as sustainable as possible in order to support the growing global demand for digitalization and sustainability. Excess heat from the server halls, for example, is supplied to a nearby bio-fuel factory. The data centers in Falun are the first data center to have a frame made of sustainable cross-laminated timber (CLT). Finally, the switch of fossil fuel to HVO fuel will further reduce the carbon footprint. By using HVO100 (Neste MY Renewable Diesel), greenhouse gas emissions can be reduced by up to 95%* when emissions over the lifecycle are compared with fossil diesel. Local pollutant emissions are also reduced, with particulate matter falling by up to 80% and nitrogen oxide by an average of 8%.

Mikael Svanfeldt, CTO EcoDataCenter, explained: “Moving away from fossil fuels is one of the foundations for a successful energy transition. With mtu emergency backup gensets and HVO from Neste, we were able to implement this without having to invest in new equipment.” The sustainable fuel is expected to continue to be used as the primary fuel for any expansions the company undertakes.

Test runs confirm high performance and safety
“Together with BOS Power and the fuel manufacturer Neste, we were able to convince EcoDataCenter, on the basis of technical analyses, documented test runs and guarantees, that our systems with HVO100 deliver the same or better performance and safety, and that maintenance intervals can be maintained. It is our strategic goal to provide our customers with reliable and efficient solutions that support them in their energy transition,” explained Tobias Ostermaier, President Stationary Power Solutions at Rolls-Royce.

Since the beginning of 2022, Rolls-Royce Power Systems has already approved 80% of its mtu diesel engine portfolio for fuels of EN15940 standard, such as sustainable HVO. For customers in the power generation sector, these are primarily the mtu Series 4000 and 1600 engines. HVO is a drop-in fuel, which means that existing diesel infrastructure can be used without any changes, and no engine hardware or software adaptations are necessary. This fuel has a significantly longer shelf life than biodiesel, which makes it even more interesting for emergency power system operators.

*The greenhouse gas emission saving varies depending on region-specific legislation that dictates the methodology for such calculations (e.g. EU RED II 2018/2001/EU for Europe and US California LCFS for the US) and the feedstock mix used to manufacture the product for each respective market.

See further information in the article Wood, HVO and a touch of Swedish romanticism: How to make data centers sustainable

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: