On a mission to cut emissions: Rolls-Royce, Porterbrook and Chiltern Railways launched passenger service with the HybridFLEX train today. It is powered by mtu Hybrid PowerPacks from Rolls-Royce. From left to right: Helen Simpson, Innovation and Projects Director, Porterbrook; David Eaton, Director Governmental Business Development & Rail, Bruce Phillips, Managing Director, both Rolls-Royce Solutions UK; Richard Allen, CEO, Chiltern Railways; Lei Berners-Wu, Vice President Global Industrial at Rolls-Royce business unit Power Systems.  Rolls-Royce, Porterbrook und Chiltern Railways haben heute gemeinsam den HybridFLEX-Zug in den Passagierbetrieb gebracht. Er wird von mtu Hybrid-PowerPacks von Rolls-Royce angetrieben. Von links nach rechts: Helen Simpson, Innovation and Projects Director, Porterbrook; David Eaton, Director Governmental Business Development & Rail, Bruce Phillips, Managing Director, beide Rolls-Royce Solutions UK; Richard Allen, CEO, Chiltern Railways; Lei Berners-Wu, Vice President Global Industrial beim Rolls-Royce-Geschäftsbereich Power Systems.
PRESS RELEASE Rail

World premiere: mtu Hybrid PowerPack from Rolls-Royce enters passenger service

Posted on February 10, 2022

Images [2 Files, 4 MB]

  • HybridFLEX train powered by two mtu Hybrid PowerPacks enters service with Chiltern Railways
  • Important step on the way to net zero mobility

Rolls-Royce, Porterbrook and Chiltern Railways are making rail history together with a climate-friendly world premiere: A hybrid diesel-battery-electric train that reduces CO2 emissions by up to 25% entered passenger service in the UK today for the first time. The so-called HybridFLEX train is powered by two mtu Hybrid PowerPacks and is operated by Chiltern Railways on the route between London Marylebone and Aylesbury. Together with the leasing company Porterbrook and Chiltern Railways, Rolls-Royce has converted a Class 168 DMU into the HybridFLEX train. The partners are proving that existing rail vehicles can be used in a climate-friendly way without the need to install complex and expensive new infrastructure. It is the world’s first regular passenger operation with mtu Hybrid PowerPacks, of which 13 have already been ordered.

Lei Berners-Wu, Vice President Global Industrial Business at Rolls-Royce business unit Power Systems, said: “It makes us proud to bring this groundbreaking propulsion solution, which we have continuously further developed over the past years, into regular service together with our partners. The immense CO2 savings based on existing and proven technologies are an important step on the road to climate neutrality, on which we are moving forward together with our customers in all applications.”

The mtu Hybrid PowerPack combines the advantages of battery and diesel-powered trains. Trains with mtu Hybrid PowerPack can also be operated on non-electrified routes purely electrically and thus locally emission-free, for example in urban areas or in stations. In pure electric operations, drive noise is reduced by about 75 percent (20 dB(A)). Important for the climate: the CO2 emissions of the train are 25% lower than those of a train with conventional diesel drive. This is made possible by the recuperation of braking energy, which is stored in a battery, the so-called mtu EnergyPacks. In the HybridFLEX, the batteries are mounted under the floor of the vehicle. A new type of driver assistance system, the mtu Intelligent Drive Manager, is being used on this train for the first time. It ensures that the drive system automatically switches to all-electric operation in emission- and noise-sensitive areas such as cities or train stations. The driver does not have to actively intervene.

“The mtu Hybrid PowerPack is an excellent example of how we are becoming a provider of integrated sustainable solutions with pioneering technologies,” said Lei Berners-Wu. Rolls-Royce business unit Power Systems, with its mtu products and solutions brand, is leading the way towards net zero as a pioneer of climate-friendly drive and energy solutions. With the sustainability programme “Net Zero at Power Systems”, the company is taking concrete steps towards climate-neutral solutions. For example, from 2023 Rolls-Royce Power Systems will approve its mtu Series 2000 and 4000 engines for sustainable fuels such as synthetic diesel (second-generation biofuels or e-diesel), thus enabling climate-neutral operation in almost all applications. In addition to hybrid systems and the use of sustainable fuels, the company is also working on future technologies such as CO2-free fuel cell systems and hydrogen engines. Digital solutions for controlling, monitoring and servicing systems are also set to help reduce CO2 emissions. 

About Rolls-Royce Holdings plc

  1. Rolls-Royce pioneers the power that matters to connect, power and protect society. We have pledged to achieve net zero greenhouse gas emissions in our operations by 2030. We joined the UN Race to Zero campaign in 2020, and have committed to ensuring our new products will be compatible with net zero operation by 2030, and all products will be compatible with net zero by 2050.
  2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 9,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids.
  3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces and navies, and more than 5,000 power and nuclear customers.
  4. Annual underlying revenue was £11.76 billion in 2020 and we invested £1.25 billion on research and development. We also support a global network of 28 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE:RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).

Contacts

Rolf Behrens Spokesman Trade Media Mobile Power Solutions
Phone:
+49 7541 90 3461
E-mail: