Two-stage turbocharging reduces contaminant emissions
It's important however not just to see the turbocharger as a 'powerpacket'. Turbocharging also helps reduce fuel consumption and contaminant emissions. A special turbocharging technique, called two-stage turbocharging, has been installed on many mtu engines in series production over the last ten years. Here, the air is not just compressed by a single turbocharger before being delivered into the combustion chamber – two turbocharger stages are used. This is particularly important on engines on which other technologies are being used to reduce the formation and emission of pollutants: e.g. the Miller process, exhaust gas recirculation systems or a diesel particulate filter. This is because these systems produce back-pressures that require compensation. With two-stage turbocharging it can still be ensured that enough air is fed to the engine.
mtu experts at Rolls-Royce are currently developing a highly compact two-stage turbocharging sytem. Here, air flows onto the turbines in axial direction, which allows a more compact turbocharger design. “This is especially important in the case of marine engines,” explained Dr Johannes Kech, head of mtu turbocharger development at Rolls-Royce.
Electrical turbocharging makes engines more agile
Electrical turbocharging can also be used to make engines more agile as well as to save fuel and enhance their eco-friendliness. With electrical turbocharging, the design weakness which is inherent to the turbocharger – at low speeds, the amount of exhaust gas arriving at the turbine is not enough to drive the compressor sufficiently – is compensated for. This insufficiency is known as the turbo lag and is made up for using electrical power. It works like this: The classic mtu turbocharger is connected to an electric drive. By using an electric drive, the operating point of the turbocharger can be made almost completely independent of the speed of the diesel engine. Significant delays in the build-up of power i.e. the turbo lag, become a thing of the past and turbocharging can take place optimally in almost any operating mode. “We've already put this technology through its paces in tests and we're expecting the first orders soon,” said Kech. Electrically powered turbochargers are primarily intended for applications where the engine is expected to deliver full power very promptly: e.g. military applications, yachts, and quick-starting gas engines used for standby power.
mtu engineers have developed a new family of classical turbo-chargers for stationary gas engines where the emphasis has solely been placed on efficiency. Unlike diesel engines used in mobile applications, power density is not all-important on the stationary gas engine. This meant that compact design was not an objective during development. “Gas engines clock up a huge number of operating hours. If we manage to raise the efficiency of these engines through highly effective turbo-charging, our customers could save a lot of fuel,” explained Kech. The new turbocharger family is to be tested in stationary mtu gas engines very shortly to demonstrate that the turbochargers can indeed raise efficiency significantly.