To be carbon-neutral, hydrogen must also be green
As a source of energy, hydrogen has a great future ahead of it. But if power delivery and power generation technology is to be truly climate-neutral, it must be produced from renewables. The trouble is, this 'green' hydrogen remains difficult and expensive to obtain. However, the European Union's Green Deal and international water strategies and programs could soon change that. Factories for mass production are currently being built all over the world and are having the effect of reducing costs.
But hydrogen is not set to be the only fuel with the potential to 'green up' the world's power delivery and power generation technology. It can be processed further into things like methanol – a fuel that is of particular interest to the shipping industry. It is easier to handle than hydrogen, and existing infrastructure can be used to transport it. The development people at Rolls-Royce Power Systems therefore also have their sights set on methanol-powered combustion engines. And as if that weren't all: using a reformer, methanol can potentially also be converted back into hydrogen which could then be used directly in a fuel cell to produce electricity.
The green energy revolution calls for everyone to pull together
“We're in the middle of an exciting transformation right now. Climate-neutral mobility and power generation is possible, and will come. From now on, it's all about teamwork. It's only by working together with our customers, partners and the politicians who create the framework that we can make the green energy revolution a reality,” sums up Peter Riegger.