High-altitude kit for deployment in Chile
lAnyone who has traveled through high mountains knows the feeling: the air gets thinner, breathing becomes difficult. The oxygen content of the air decreases with every meter of ascent. Anyone used to hiking at altitude would not notice too much difference at 3,000 meters or so. However, those of us used to lowland areas may well experience breathing difficulties at 1500 meters. And the situation is the same for the Leopard 2 tanks which have formed the backbone of the Chilean army for the last three years and which have to deliver top performance at altitudes up to 4,300 meters. This presents a particular challenge for the vehicles’ turbochargers which increase their speed but still feed less combustion air into the engine. As a result, exhaust temperature rises and the service life of many components decreases. To stop this happening, a new compressor wheel in the turbocharger acts together with the sensors in the exhaust temperature monitoring system to ensure that the engine does not overheat and engine output is throttled back almost unnoticeably. In this way, the engine is able to deliver the high levels of performance demanded of it, even high up in the mountains.
Crashing waves, biting spray and freezing temperatures. Lifeboats are usually called out when the wind is at its strongest, the waves at their highest and other vessels cannot cope with the conditions. So that the lifeboats do not become rescue cases themselves, they are self-righting in case they capsize. “We design our engines specifically to cope with such extreme conditions and to make sure that there is always enough oil available to coat the moving parts with a lubricating film, we also test them on a special tilting test stand,” explained Dr Carsten Baumgarten, Test Team Leader for Series 2000 engines. The engines are tilted over at angles up to 45° on the special test stand and subjected to all load and speed combinations. The tests enable the developers to answer questions such as what the oil pressure is, how much air there is in the oil or how much oil there is in the engine’s blow-by, which is fed back into the intake air via the crankcase venting system. Engines that are used in haul trucks or excavators have to be able to operate at inclinations up to 15° in any direction. For marine engines, that figure is significantly larger in some cases. In armored vehicles, some mtu engines are required to operate at inclinations as extreme as 45°. To do so, they are equipped with a special type of drysump lubrication system. The oil is pumped continuously from the sump into a smaller reservoir from which it is delivered to the engine. This ensures that sufficient oil always reaches the engine lubrication points.