That’s not to say there wasn’t some initial concern about the switch, as Hoffman explained:
“When we first began using R99, we entered into a dialogue with Rolls-Royce’ Power Systems business unit. They initially did not accept the R99 on their approved fuels list. But they were interested in working with us to find out how R99 interacted with their engines, particularly the fuel system: low-pressure and high-pressure fuel pumps, fuel injectors, and fuel filter seals. As a result of these discussions, Rolls-Royce agreed to work with us, removing the identified fuel system components from a few of our vessels that had accumulated more than 3,000 hours on R99. These components were returned to the factory for further evaluation, as part of Rolls Royce Power Systems standard fuel release process. It was a very positive process for both companies.”
What is renewable diesel?
HVO is produced from waste vegetable and animal fats and used vegetable oils. These base materials are converted into hydrocarbons that can be used as a substitute for fossil fuels, such as diesel, via a catalytic reaction with hydrogen. The resulting fuel not only significantly lowers PM emissions by up to 80%; it reduces emissions of other harmful pollutants, including nitrogen oxides (NOX) by up to 8%.
The use of HVO also reduces carbon emissions. Because the production, transportation, and combustion of renewable diesel only emits about as much carbon dioxide (CO2) as is absorbed by the biomass base materials during growth, the use of renewable diesel results in a significant reduction in carbon footprint. CO2 emissions can be reduced by up to 90% compared to traditional fossil diesels. Renewable diesel thus has significant implications for the decarbonization of hard-to-abate sectors, such as the marine industry.
A final – but important – benefit to note is that the production of renewable diesel doesn’t compete with food production, because it relies only on waste and residual biomass as base materials.