South of the equator, on the western Indian Ocean, the Seychelles are located in a tropical idyll. With its dream beaches, the archipelago is considered a holiday paradise. But climate change does not stop at an island paradise - rising sea levels and increasingly extreme weather events threaten the existence of the small islands. In order to preserve the idyll in the long term, sustainable solutions must be created. To this end, the island nation is relying on green energy: a 50,000 square metre solar park with a total output of 6 megawatts was built on Île De Romainville in front of the capital Victoria on Mahé. In addition, there are five wind turbines with an output of 750 kilowatts each.
Previously, electricity on Mahé was generated almost exclusively from fossil fuels. Now, the huge solar park and wind turbines ensure that seven million kilowatt hours of green electricity are generated every year - enough for around 2,000 households.
mtu EnergyPacks stabilise the grid when the sun is not shining
"The Seychelles, with its many hours of sunshine and exposed location, is the ideal location for photovoltaic systems and wind turbines," says Alexander Wahlig, Senior Systems Engineer at Rolls-Royce. But even in the island paradise, the sun does not always shine and the wind does not always blow. This leads to fluctuations in electricity production which poses stress on the power generators and utility grid. "And that's where our mtu EnergyPacks come in," says Wahlig. With an output of 5,100 kVA and a storage capacity of 3,363 kWh, they ensure that the fluctuations in generation are balanced and the security of supply is increased.