USCG Fast Response Cutter FRC_2x20V4000 M93_mtu (1).jpg
PRESS RELEASE Naval Solutions

Rolls-Royce to power additional Fast Response Cutters with mtu engines

Posted on April 21, 2026

Images [1 Files, 2 MB]

  • Additional cutters support modernization of the U.S. Coast Guard fleet and expand its maritime mission
  • Longtime Rolls-Royce customer Bollinger Shipyards awarded expanded contract for construction of the vessels; secures hundreds of U.S. jobs

Rolls-Royce has been selected to supply its mtu 20V 4000 M93L engines for ten additional Sentinel Class Fast Response Cutters (FRCs) ordered by the U.S. Coast Guard (USCG), which expands the total program order to 77 ships. Each vessel will be powered by two 4300 kW (5,766 HP) mtu Series 4000 engines, enabling speeds of more than 28 knots. Bollinger Shipyards of Lockport, Louisiana was awarded the construction contract for the new FRCs, which will sustain 650 jobs in Lockport and support a national industrial footprint spanning numerous U.S. states.

Bollinger has already delivered 61 FRCs equipped with mtu 20V 4000 M93L engines. The original contract was for up to 58 vessels, with final delivery set for 2028. Extensions to the contract increased the program to 77 cutters and extends the production line by approximately three years.

The new FRCs will help modernize the current USCG fleet – creating a more agile, capable and responsive fighting force – and will complement the capabilities of the USCG’s other security cutters as an essential element of the nation’s layered maritime security strategy. 

Designed for high-demand marine applications, Rolls-Royce’s mtu 20V 4000 M93L engines offer high-power density, compact design and exceptional fuel efficiency, allowing the FRCs to significantly increase their mission durations and range, reach high speeds, and achieve optimal performance in demanding maritime conditions. Rolls-Royce will also provide ongoing service support and maintenance for the engines throughout their operational life.

Rolls-Royce has a long-term customer relationship with Bollinger, having supplied propulsion technologies for multiple USGC vessel platforms built by the company over the past 30+ years. 

Scott Hanson, Vice President, Governmental Sales North America for Rolls-Royce’s Power Systems Division said: “We are proud that our longtime customer Bollinger has placed its trust in us and our mtu engines for the extension of the USCG FRC program, which supports jobs across the U.S., including at Rolls-Royce. Together, we have delivered the proven performance and reliability that enables the Coast Guard to achieve its mission, supported by an experienced maintenance and service team. We look forward to continuing to support our national security with these additional vessels.”

Since their introduction to the USCG fleet in 2012, Fast Response Cutters have consistently proven their capability, adaptability and effectiveness in a wide range of maritime environments and missions, including law enforcement, search and rescue, fisheries protection and national defense. 

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Jennifer Riley Spokeswoman North and Latin America
Phone:
+1 248 560 8488
E-mail: