mtu power system supplies building’s 800 kW load
The vehicle maintenance facility is 38 feet high and more than 600 feet long and includes four different types of rail track: a component removal track, designed for repairs on two cars at once; a larger repair-and-maintenance track; a storage-and-inspection track; and a train-wash track, located in a separate building. The building’s electric loads include HVAC, lighting and electrical service to the administrative offices, but the majority of the load is for largescale industrial equipment for the ongoing maintenance and repairs performed on the cars and engines. This includes truck hoists and a wayside power cabinet for the component removal track. Wayside power provides heating, lights and ventilation to trains when they are not powered by the diesel-electric locomotive. The train wash alone is 20 percent of the load.
The 1,000 kW mtu power system includes an mtu 16V2000 engine with 1,495 brake horsepower, a 480-volt alternator and transfer switch. The Series 2000 engine features an advanced diesel engine controller, or ADEC, that optimizes combustion and allows the engine to meet current exhaust emissions requirements. “In the event of a utility power outage, the generator will assume the load within 10 seconds of power loss,” said Clarence Cronin of Design Electric, St. Cloud, Minnesota, the project’s electrical contractor.
“We call the Series 2000 a workhorse generator set because of its reliability,” said Stalpes. “This mtu power system is designed for robust applications that need dependable electrical power.” The generator set is located outside of the facility and housed in an aluminum enclosure for added corrosion resistance. A 1,400-gallon fuel storage tank provides up to 24 hours of running time.
Interstate Power provides training
“Most customers look to us for generator system maintenance,” said Stalpes, “but a small percentage of customers conduct their own maintenance when they are equipped and trained for it. Since Northstar trains are dieselelectric units, the maintenance facility has the equipment, personnel and training to maintain the generator set, including regular inspections and exercise. In this case, Interstate Power Systems provided training and operational protocol, and we are always available for assistance when needed.”
The Northstar Rail Corridor is one of the fastestgrowing transportation corridors in Minnesota and the nation, creating an alternative way for people to commute. Passengers will judge their new service mostly on its on-time arrival. The mtu power system is “on track” to meet that need.