PRESSEMELDUNG

ROLLS-ROYCE PRESENTS EXTENSIVE ENGINE AND SERVICE PORTFOLIO FROM mtu AT BAUMA CHINA

Veröffentlicht am 22 November 2016

Rolls-Royce is showcasing its extensive construction and industrial portfolio from mtu at this year’s Bauma China in Shanghai from 22 to 25 November 2016.

Bilder [1 Dateien, 3 MB]

  • mtu EU Stage V engines on display at Bauma China for the first time in Asia
  • Emission Flex Package enables diesel engines to be used in countries with different emission requirements
  • mtu ValueCare offers a wide spectrum of services to maximize uptime and performance of mtu products

SHANGHAI, CHINA – Rolls-Royce is showcasing its extensive construction and industrial portfolio from mtu at this year’s Bauma China in Shanghai from 22 to 25 November 2016. mtu’s booth number 451 is located in hall 5 at the Shanghai New International Expo Center (SNIEC). mtu will be presenting a portfolio of products in the 75 to 3,000 kW range. Featured at the booth will be the Series 900, Series 1500, Series 2000, in addition to the associated exhaust after-treatment system. The mtu brand is part of Rolls-Royce Power Systems.

For more than 100 years, mtu has offered an extensive product portfolio covering applications for ships, heavy agricultural, rail and military vehicles, as well as the oil and gas industry. For C&I applications, mtu’s versatile engines are primarily valued for their low fuel consumption, outstanding power coupled with compact design, impressive dynamic performance and excellent availability. As engine requirements become more demanding, mtu stays persistent in its credo of – “Tougher - Whatever The Conditions” – proving the superiority of mtu engines on a global scope.

mtu joined together with Daimler to bring engines on EU Stage V level


With engines ready for existent EPA Tier 4 markets mtu will explain its latest cooperation with Daimler to further develop the mtu 1000 – 1500 Series based on Daimler commercial vehicles making them compliant with the forthcoming EU Stage V emission regulation. With power outputs from 100 – 480 kW mtu engines meet the new EU Stage V emission limits, which will also apply to soot particles, by using advanced internal engine technology, an SCR exhaust gas after-treatment system and an additional diesel particulate filter. The 6-cylinder Series 1500 engine will also be on display, in addition to the associated exhaust after-treatment system.

Emission Flex Package from mtu provides vehicle operation worldwide


With regards to varying emissions standards around the globe mtu will also present the Emission Flex Package, an innovative solution enabling customers to operate engines in countries where different emission requirements apply. Engine systems that to date have been developed solely for markets with stringent emission regulations with exhaust gas after-treatment, can now be operated outside these highly regulated markets as well and create value to transfer those machines possibly to those countries where different emission regulations apply.. Customers will benefit from this new feature as it allows to sell the vehicle in numerous countries without changing or modifying the vehicle, which usually results in high costs and time-consuming procedures.

The Emission Flex Package will be offered as a retrofit solution for Series 900, 460 and 500 engines based on Mercedes-Benz classic engine series, designed to meet China 3, EU Stage IIIB and Tier 4 interim. For new engines, the Emission Flex Package is planned for EU Stage IV and Tier 4. This means that mtu provides engines for all areas of application within the construction industry that need to meet very different emission requirements.

Engines for the power range above 500 kW


For above 500 kW there are mtu’s Series 1600 engines which are available for the 567 to 736 kW power range. In addition to complying with the US EPA Tier 4 emission regulations, they are also designed to meet the future EU Stage V regulations using internal engine technology. No exhaust aftertreatment is required.

mtu will also have a 12-cylinder Series 2000 engine on display at Bauma China. The mtu Series 2000 engines for installation in construction and mining equipment cover a power range extending from 567 to 1,163 kW and are available for EPA Tier 4 interim emission regulations. For Series 2000, it has been planned to obtain the China 4 certification by 2017.

In addition, mtu offers 12, 16 and 20-cylinder Series 4000 models with power outputs extending to 3,000 kW. They meet the China 3 certification and also US EPA Tier 4 emission regulations with no exhaust gas aftertreatment, depending on the engine model.

mtu ValueCare offers complete lifecycle support.


mtu supplies not only the engines, but also the system expertise and localized service to match the customer’s needs. The mtu ValueCare service portfolio includes customised maintenance solutions, rapid supply of spare parts and consumables such as engine coolant, engine oil and filters and also remanufactured engines and parts to ensure peak performance, long life and optimised costs throughout the entire lifecycle of mtu equipment. Due to mtu’s extensive network of authorized distributors and service dealers, mtu ValueCare products and services are available throughout the world.
Peter Knoop Sprecher Asien
Tel.:
+65 6860 9448
E-mail: