Peter bought the Olympia in 2008 and is impressed with its performance. “We once ran at about 1500 RPM with tremendous noise and did around 9 MPH,” Peter boasts. “And at 1000 RPM, fuel consumption is only 6 liters an hour.” Peter has not experienced any oil leaks and is pleasantly surprised by the easily accessible parts supply and service offered by mtu.
The sound of a jimmy is music to Peter’s ears, especially when open water beckons. “Holland is a relatively small country, we don’t always have the possibility to go full throttle,” Peter says. “So once you can, especially at night through the main canals, you really can see fire coming out of the exhaust, and she runs like hell.”