A marathon with a difference
At this year's Olympics, almost nothing will be the same: Ringer's destination will not be Tokyo, the main Olympic venue. He'll be travelling directly to Sapporo, where he will be accommodated in a hotel. There will be no Olympic village. The marathon itself will take place largely out of the public eye, with spectators not likely to be permitted. The athletes will not run across the city as usual, but around circuits, the largest of which will be 22.195 m, with two smaller circuits of 10,000 m. Richard could turn that to his advantage, however, since the 10,000 m discipline was his specialty. “My 10,000 m background has given me a capacity to sprint that not every marathon runner possesses,” he explained.
“Running a marathon has a much bigger psychological aspect than running long-distance along a track,” explained Ringer. Obviously, what counts first and foremost for any marathon runner is making it to the finishing line, but other difficulties have to be factored in as well. Ringer divides the race into 5-km stretches, for each of which he sets his own time targets. The marathon runner's battle begins at around 30 or 35 kilometers, when a heaviness in the legs sets in. “It starts to be more about your mental strength, and you have to stay completely focused.”
All-round motivation
The main source of motivation for Ringer is his normal everyday life. “My big advantage is that my employer and co-workers are ready to free me up,” said Ringer. With a part-time job in business controlling, he has a steady income that allows him to concentrate on his running. “When I'm not competing, I'm in the office. That can be for a matter of months or a matter of hours. But when I'm there, my mind is completely on the job. And being at work with my colleagues give me a great sense of equilibrium. I experience a kind of calmness and lightness of touch there that I can put into my running,” he explained. That's why the question of whether the Olympics would actually happen in 2021 or not never really worried him. He simply kept to his training schedule for a race on 8 August. At worst, he would be able to run a marathon elsewhere.
So Ringer stays focused on the 8 August. His aim is a good finishing time in Sapporo. And he'll be back at work in August doing business controlling, but with a fresh set of plans – one of the big city marathons, where he'll be running down the straight rather than a circuit, with friends and spectators there to cheer him on. Then follows the next Olympic Games in Paris in 2024. Richard Ringer has a full agenda.