Antriebssysteme sind heute so komplex, dass zu deren Betrieb und Wartung große Mengen an Informationen nötig sind. MTU liefert diese Daten in digitaler Form.
故事

Forget the files and tap the app

发帖 2017年1月18日, 图片拍摄者 Robert Hack, Rolf Behrens

Huge amounts of information are required to run and maintain complex drive and propulsion systems . mtu supplies this information in digital form.
Friedrichshafen, Germany

Today’s drive and propulsion systems are so complex that huge amounts of information are required to run and maintain them. mtu also supplies this information
in digital form. Increasingly, printed operating instructions are being supplemented with helpful 3D videos.

The sophisticated animation captured many people’s imaginations at the Eurosatory military equipment fair in Paris, where the product made its début.

A very ordinary flat-screen display stole the show from the genuine PowerPack in the Puma infantry fighting vehicle at the ‘Eurosatory’ military equipment trade fair in Paris.
The powerful drive system was actually the dominant feature on the mtu stand. But for visitors from near and far, the star of the show was a display on the monitor behind it: a highly detailed, almost hyper-realistic 3D animation of the Puma PowerPack, which was making its world début at the fair.It was giving a kind of x-ray view, drawing the audience into an amazingly true-to-life journey through the inside of the engine. Delegates from all over the world were able to follow the flow of air through the various components and view, in amazement, the movements of pistons, valves and turbine blades which otherwise remain hidden from view. Despite weighing many tons, the drive system was able to be moved around on-screen and flicked over in any axis, and individual sub-assemblies enlarged.

Learning more effectively with 3D


The latest product from the team run by Ulrich Korioth – responsible at mtu for technical documentation for government projects – really caught the imagination of many visitors to the trade fair. “The interactive model showing the workings of the Puma PowerPack was something we created for the German Armed Forces,” explained Korioth. “They are using it at the Land Systems Engineering Training Center in Aachen for training soldiers in the maintenance corps.”
Ulrich Korioth and his team use Smart Factory revolution principles to create leading-edge working images and operating instructions.

The software enables incredibly vivid explanation of how the drive system works – with details and perspectives which would never be possible using the physical machinery. In addition to showing the working principles, the dynamic processes at work inside the engine can also be depicted, for example, at various different engine speeds. Future projects will also include showing what happens when malfunctions occur. Learning efficiency is boosted, as every single bolt and cable looks exactly like it does ”in the flesh“ and is shown in realistic detail hitherto unknown.

3D videos support heavy-duty strategies


However, Korioth and his team are able to do much more than just demonstrate how a drive system works in 3D: maintenance and repair of mtu engines are also made simpler and easier for the customer using products created by Technical  documentation. Used as part of a maintenance system like Callosum MT, developed by mtu for the shipping industry, ships’ crew can perform scheduled maintenance or
necessary repair activities after watching them in 3D videos: say a coolant pump has to be replaced, the system shows the mechanic exactly which bolts need to be removed and where, and which tools, spare parts and consumables will be needed.
The German Armed Forces are using the interactive program to train soldiers. It helps explain all the workings of a drive system in an easy-to-follow way – including x-ray views of the interior.

Like a YouTube tutorial


These instruction films are sure to remind younger mechanics of tutorial videos on YouTube and other video websites, because that is where they go for easy-to-follow instructions on practically everything – from changing a bicycle tube to making car repairs, or even knotting their neckties. Thanks to such films, even less experienced naval mechanics are able to carry out quality maintenance work without losing much
time. These mtu maintenance animations are the modern answer to challenges facing many customers. Financial cuts and skills shortages mean that the same number of vehicles and machines have to be run and maintained by fewer and fewer people – at the same time as dealing with growing system complexity and what are often restrictive working hours policies. The German Navy, for example, is operating
a heavy-duty strategy on its new Class F125 frigates, deploying the vessels for two years without interruption and with crew changes every four months. This is made possible, among other things, by the long maintenance intervals of the mtu engines aboard – and by the use of Callosum MT with its 3D maintenance tutorials.


As if the rest of the engine were made of glass: individual sub-assemblies can be enlarged and animated while running at different engine Speeds.

The Smart Documentation revolution


Conveying knowledge about how a drive or propulsion system works and how it should be maintained is both a conventional and a highly up-to-the-minute task for the
mtu Technical Documentation unit: “What we’re doing is the epitome of the Smart Factory revolution,” said Ulrich Korioth. “We connect customer and information, ensuring it is to hand at the right moment in a form he can actually use.” For the customer, this is often a key aspect when purchasing a drive system.

On request, mtu provides all data in digital form in such a way that it can be transferred to customer systems and connected to other sources of information – such as a vessel’s master logistics system. The conventional hard-copy operating instructions are now just an ancillary item to be used as backup. Very soon, mtu instructions could become available as apps for mobile cell phones and tablets, etc. This carries a lot of customer benefit: I nstructions do not just become easier to follow, they can also be integrated with digital systems used by the customer – not to mention
making today’s pallet loads of paper a thing of the past. “When creating digital documentation, the number one rule is to take a standardized approach to capturing the data,” explained Ulrich Korioth.

Even the fuel can be followed all the way from the tank to the combustion chamber. Pipework turns see-through at the click of a mouse button, with different fuel pressures shown in different Colors.

Each piece of information is specified – “keyworded”, you might say – using a consistent system. Indeed, ever since the year 2000, mtu has been observing international digital standards used in industrial and military environments such as the German Armed Forces. Observing uniform specifications ensures information can be reused easily within various different digital systems and is able to be fully integrated as required. The same goes for the 3D models mentioned above. This reusability is one of the key prerequisites for making the Smart Factory revolution work. “This technological development means mtu’s technical documentation is right up there at the cutting edge,” said Korioth.

Youtube Video


联络点

Ulrich Korioth
电话:
+49 7541 90 2902
+49(0)7541 902902
传真:
+49(0)7541 90902902
电子邮件:

相关故事

发电

Enabling the future with microgrids

Microgrids combine the advantages of renewable energies with the stability of conventional power generation systems.

了解更多内容

Combustion engines remain our core specialty

The combustion engine is the core component of mtu systems and it will continue the companies great passion.

了解更多内容

Why hybrid drives are the future

Hybrid drives connect two worlds: clean travel powered by electric motors and long-distance travel powered by combustion engine technology.

了解更多内容

公司

“We don't just do diesel”

Andreas Schell explains how the company is to stay at the cutting edge of drive and propulsion technology.

了解更多内容