Iarnród Éireann Irish Rail and Porterbrook order a total of 13 MTU Hybrid PowerPacks
故事 铁路

mtu celebrates initial orders for its hybrid rail drives

发帖 2019年4月16日, 图片拍摄者 mtu

Iarnród Éireann Irish Rail and Porterbrook order a total of 13 mtu Hybrid PowerPacks
United Kingdom

mtu has achieved a pioneering breakthrough for hybrid rail drive systems: Both Iarnród Éireann Irish Rail, the state railway of the Republic of Ireland, and Porterbrook, the UK’s largest rolling stock leasing company, have signed contracts with mtu to supply Hybrid PowerPacks. By doing, the companies have converted commitments made in September 2018 at Innotrans, the world’s largest railway trade fair, into firm orders. Iarnród Éireann Irish Rail has ordered nine mtu Hybrid PowerPacks, with Porterbrook initially taking four. The Hybrid PowerPacks are to be delivered between May 2020 and the end of 2021. Both customers are evaluating the possible conversion of significant parts of their fleets to hybrid once successful trials of this cutting-edge technology are completed.  

Jürgen Blassmann, Head of  Rail Business at mtu, said: “We are proud to see the mtu Hybrid-PowerPack, which we’ve been pioneering for years, now establishing itself in the market as a leading-edge traction solution. These first orders are a milestone as we transform the company from an engine and PowerPack manufacturer to a solution provider offering tomorrow’s sustainable traction systems.”

mtu’s Hybrid PowerPack is an environmentally friendly drive system that combines the benefits of battery-powered and diesel-powered traction systems. It combines an mtu diesel engine, built to EU Stage V requirements, with an electric unit that can function both as a motor and as a generator, and with the mtu EnergyPack battery system that stores energy recovered during braking. This enables, among other benefits, operations with zero local emissions under battery power. In station areas, traction noise is reduced by around 75% (20 dB(A)). Consumption and CO2 emissions are cut by up to 25%. Operating costs of vehicles fitted with hybrid drives are also significantly lower, and even brake pads and discs have reduced wear due to brake energy recuperation. As a result of the additional power of the electric machine, train operators also have the option to improve journey times through better acceleration.
 
mtu has brought this technology to full-production maturity in recent years, making ongoing refinements. For this pioneering work, mtu has now also received the Innovation Prize awarded by German rail sector publishing house Bahn-Media-Verlag: The mtu Hybrid PowerPack scooped the prize in the Energy and Environment category for its contribution to climate protection and resource conservation.   

The content of the stories reflects the status as of the respective date of publication. They are not updated. Further developments are therefore not taken into account.

联络点

Manfred Martin Gössler
电话:
+49 7541 90 7634
+497541907634
电子邮件:

相关故事

铁路

Cruise Train on rails

Superlative in every respect, the Train Suite Shiki-Shima is powered by electricity generated by two mtu Series 4000 engines on non-electrified routes.

了解更多内容

铁路

Destination Gotthard

Railcars from Harsco Rail, powered by mtu PowerPacks, will play a key part in maintaining the world's longest railway tunnel.

了解更多内容

铁路

专用轨道车辆

了解更多内容