GranjasCaroll_1.jpg
故事 发电

Reliable off-grid power supply

发帖 2021年3月23日, 图片拍摄者 Matt Hieber Productions

Self-sufficient energy supply: Granjas Carroll pork processing plant has a state-of-the-art independent power plant.
Oriental, Mexico

Sitting 8,000 feet (2,400 m) above sea level, the quaint town of Oriental in rural Puebla state, Mexico is surrounded by untamed mountain wilderness, scenic farming valleys, and charming Mexican villas. It is also the location of a Granjas Carroll pork processing plant that is a state-of-the-art powerhouse of production.

As part of one of the country’s largest pork producers, the Granjas Carroll facility has the capability to process 1.5 million hogs per year. With such a heavy rotation of output, having reliable, consistent energy with no fluctuation in voltage or frequency is critical. But when the plant was first being built, having reliable power – or any power at all – was an uncertainty. Under the initial plans, the new facility was to receive service from the local electricity company. As the project got underway, word suddenly came that the local provider would not be able to provide power after all.

This left the project managers in a scramble to construct a completely independent power plant, one that could operate off the grid in full island mode and produce enough electricity reliably enough to handle all the plant’s refrigeration and auxiliary needs. That’s when the Granjas Carroll team reached out to local distributed energy systems expert Electriz, S.A. de C.V. to assist them in designing a solution and to lead the engineering, procurement and construction of the power plant project. Based on the specific needs of the plant and its 24/7 energy requirements, the experts at Electriz decided to suggest four mtu Series 4000 gas generator sets and one mtu Series 4000 diesel generator set, all operated under one overall control system to power the plant. 

Youtube Video

This resulted in the first off-grid solution of its kind in the Americas for Rolls-Royce Power Systems, manufacturer of the mtu products. Constructed in just a few short months, the facility went online in late 2018 and has enjoyed continuous, uninterrupted power ever since. “There were multiple factors beyond reliability that needed to be considered when deciding on power solutions for this facility,” said Daniel Salazar, President, Electriz. “Cost-effective efficiency at that altitude, while also taking environmental factors into consideration, is difficult. However we knew that by working with Rolls-Royce, we could get it done.”

“We have a vision at our company to be the most recognized and most preferred pork company in Mexico,” said Rafael Patino, Director of Environment & Energy, Granjas Carroll. “That is a big challenge and sustainability is one of our pillars of production, so our project came with very demanding specifications.” The four gas units used at the facility are 20-cylinder Series 4000 natural gas systems delivering altogether 7.7 MW of electrical power, capable of handling the pork processing facility’s altitude demands with the lowest derating, ensuring maximum power availability at the site. In a second phase, it is planned to use the heat out of the exhaust gas, the oil cooler and the mixture cooler to efficiently produce steam and hot water, which can then be used in the production processes.

A single 16-cylinder Series 4000 diesel generator system with an electrical output of 2 MW is tasked with absorbing greater load blocks than the natural gas units, offering long-term stability to the plant. The diesel unit will run continuously with loads as low as 10 percent to minimize fuel consumption, allowing the natural gas units to produce more energy. An mtu MCS master control panel integrates plant control and remote operation, and all systems run in isolation from the power grid, providing reliable, stable and efficient electrical power to the entire facility. 

“This plant has to rely 100 percent on its own grid, so the challenge was to deliver a complete solution that would ensure grid stability at a high level,” said Alfredo Carrasco, Latin American Senior Sales Manager, mtu Onsite Gas Systems. “The reliability and efficiency of our systems, along with the ability of our team to meet the stringent requirements of gas, diesel and an integrated control system from a single supplier were major factors in us supporting this project.” With the help of the flexible mtu systems, the plant will have the ability to double its capacity in the future – even connecting the power plant into the grid to provide additional power to the surrounding community. “With the success of this project, we now have the goal to eventually operate our power plant on the grid,” said Manuel Rodriguez, Energy Specialist, Granjas Carroll Mexico. “mtu’s technology is a key factor in us achieving this, and it will allow us to increase our power generation and provide sustainable and clean energy to our neighbors.”

At a later stage there are also plans to use biogas from livestock waste as another source of fuel to operate the plant. “There are a lot of good companies out there, but when you have a problem and a company proves that it is dependable, quick and thorough in responding, you don’t want to do business with anyone else,” said Salazar. “The name of the game in the power generation business is both efficiency and availability, and mtu’s solutions offer both.” 

Lone island: Granjas Caroll has set up a state-of-the-art production plant with its own power supply.
Four 20-cylinder mtu Series 4000 natural gas systems deliver 7.7 MW of electrical power in total to cover basic requirements. A 16-cylinder series 4000 peak-shaving diesel genset ensures long-term stability
Straightforward genset monitoring: The plant and remote control systems are integrated in an mtu-MCS main control panel.
Granjas Caroll processes a good 1.5 million hogs per year in Oriental alone.

This plant has to rely 100 percent on its own grid, so the challenge was to deliver a complete solution that would ensure grid stability at a high level.

Alfredo Carrasco, Latin American Senior Sales Manager for gas systems at Rolls-Royce
发电

Interview with Chris Pritchard on sustainable solutions and AVK's experience with HVO fuel

Rolls-Royce and AVK now provide over 3.5 gigawatts of backup power in the UK. Data centers and the financial sector are increasingly turning to sustainable solutions. In this interview, Pritchard talks about the trends he sees here and his experience with the use of the sustainable fuel HVO.

了解更多内容

发电

Walking the journey to Net Zero together

At the mtu Power Generation Symposium, experts discussed how mtu solutions are helping to master the energy transition.

了解更多内容

发电

面向未来港口物流的氢基能源

杜伊斯堡港将成为欧洲首个实现气候中和的内陆集装箱码头,这要归功于mtu氢基动力解决方案。

了解更多内容

Connect with Us

Customer Assistance Center

We are here to take your Sales & Service questions around the clock, 365 days a year.

了解更多内容

Sales & Service Locator

Find your local partner for Sales & Service.

了解更多内容

mtu Stories

Reports and interviews about mtu products and solutions.

了解更多内容