故事 商用船舶

Rolls-Royce powers record-breaking vessel in China

发帖 2021年7月27日 由 Julia Rieß, 图片拍摄者 Aulong Shipbuilding

BeiYou26 is a national record-breaker in more ways than one. 70.6 m long and 17 m wide, the vessel can accommodate 1,200 passengers and is the largest ferry with aluminum hull ever to have been built in China. The vessel is powered by 16-cylinder mtu-brand Series 4000 units.
Weizhou Island, China
The Chinese island Weizhou covers some 25 km2 and is the biggest volcanic island in China. It has some 16,000 inhabitants and is a favorite destination for short holiday breaks. Since July 2020, the largest catamaran ferry ever built in China has been shuttling islanders and tourists between Weizhou and the mainland and is propelled by powerful mtu Series 4000 units. 


Weizhou Island lies in the Gulf of Beibu in the north-west South China Sea. From Beihai in Guangxi province on the mainland, the sea route stretches some 35 km south towards the island.  Since 22 July 2020, this journey can be made more quickly and comfortably than ever a new high-speed catamaran that plys between the mainland and the island. 

The vessel is a national record-breaker in more ways than one. 70.6 m long and 17 m wide, the vessel can accommodate 1,200 passengers and is the largest ferry with aluminum hull ever to have been built in China. Equipped with unique features such as leather massage seats and a special area for domestic pets, the BeiYou 26 is unrivalled when it comes to comfort and convenience.  Besides the comfort, passengers also appreciate the speed at which they reach their destination.  Shipyard Aulong Shipbuilding opted for 16-cylinder mtu-brand Series 4000 units from Rolls-Royce, capable of speeds up to 34 knots or 63 km/h. These units count among the most renowned high-speed engines ever, as Richard Wang, head of Marine Sales at mtu China explained: “These engines also carry the name 'ironmen' due to their incredible robustness,” he explained. Series 4000 units are famed for their power, reliability and long service life. Another major advantage they boast are low operating costs. 

Shipyard Aulong Shipbuilding opted for 16-cylinder mtu-brand Series 4000 units from Rolls-Royce, capable of speeds up to 34 knots or 63 km/h.

Rolls-Royce Power Systems brand mtu successful in China 

mtu-brand engines have won the confidence of Chinese shipping companies. At the third China International Import Expo (CIIE) exhibition in November 2020, the Rolls-Royce business unit Power Systems signed a partnership agreement with the Jianglong and Aulog shipyards. Jianglong Shipyard is the leading Chinese shipbuilder of high-speed vessels with aluminum hulls. Aulong Shipyard is shipyard with international design focus on high speed ferry and long-standing business partner of Rolls-Royce Power Systems and Jianglong. The new strategic partnership focuses on mtu Series 2000 and 4000 marine engines. 

商用船舶

"Green methanol" will power innovative mtu marine engines

由 Peter Thomas

Heading for the future with e-methanol: Rolls-Royce develops high-speed mtu methanol engines as a game-changer for climate-friendly shipping.

了解更多内容

商用船舶

When the day comes ...

由 Lucie Maluck

It doesn't always have to be a new engine: With Insitu and Reman, marine customers have several options for a major engine overhaul, saving time, money and resources.

了解更多内容

商用船舶

Ferry efficient – reliable transportation to the island of Helgoland

由 Anne-Katrin Wehrmann

Since going into service in April 2018, the high-tech state-of-the-art catamaran Halunder Jet has developed quite a reputation for its fast, smooth ride across the German Bight. The vessel plying between Hamburg and Germany's only deep-sea island now has the benefit of another piece of innovative technology: the new mtu NautIQ Foresight equipment health management system.