Rolls-Royce's new intelligent crew support systems mtu NautIQ CoPilot, mtu NautIQ CoOperate and mtu NautIQ CoDirect offer different levels of intelligent crew support, autonomous control, and remote command capabilities. They are powered by Sea Machines technology. Die neuen Rolls-Royce-Produkte mtu NautIQ CoPilot, mtu NautIQ CoOperate und mtu NautIQ CoDirect bieten Kunden unterschiedliche Möglichkeiten zur intelligenten Crew-Unterstützung, autonomen Steuerung und Fernbedienung von Schiffen und deren Funktionen. Sie basieren auf Technologie von Sea Machines.
新闻稿

Rolls-Royce launches new mtu NautIQ products with Sea Machines technology to deliver intelligent crew support systems

发布于 2022年4月05日

图片 [1 文件, 2 MB]

  • Rolls-Royce offers three new mtu NautIQ products with different levels of intelligent crew support, autonomous control, and remote command capabilities 
  • Important contribution to safety, efficiency, and net zero targets 
  • Powered by Sea Machines technology 

Rolls-Royce is expanding its range of mtu NautIQ ship automation systems with three new products: mtu NautIQ CoPilot, mtu NautIQ CoOperate and mtu NautIQ CoDirect, which each offer different levels of intelligent crew support, autonomous control, and remote command capabilities. Customers in all marine applications will gain significant operational advantages and benefits in terms of safety, efficiency, environmental impact, and climate friendliness. The new products are the next step in the cooperation between Rolls-Royce and Sea Machines Robotics, the leading developer of autonomous control and remote-vessel command systems, which was first announced at Monaco Yacht Show in September 2021. The continued development of the mtu NautIQ product range is at the core of Rolls-Royce’s strategy to be an innovation leader in the marine business and to provide customers with complete propulsion and control solutions from ‘bridge to propeller’. 


mtu NautIQ CoPilot is the most advanced intelligent pilot assist system of the new product range. Depending on operating mode, the human-on-the-loop system can either autonomously control a planned voyage from start to finish, or not intervene at all in human operations, while only guiding the operator. The system enables navigation with greater precision and predictability, helping to reduce costs, fuel consumption and emissions. It is an important step towards more climate-friendly marine operations, made possible by the groundbreaking fusion of digital marine sensors, embedded electronic charts, advanced AI algorithms and one of the world’s most advanced broad-area computer vision systems. 

mtu NautIQ CoOperate is an optionally autonomous ship navigation command system which enables off-boat remote command, including all payloads on board. The system can take over routine and monotonous vessel tasks and it allows crews to focus on more important aspects of their missions. The system has recently proven itself in the field in spectacular fashion: The tug Nellie Bly used the system to complete a 1,000 NM roundtrip from Hamburg around Denmark, remotely commanded from an office in Boston, USA, 3,000 NM away. As with all the new products, operators can intervene at any moment if necessary.


mtu NautIQ CoDirect is a wireless, remote-helm system that can control a vessel’s engines, steering and transmission as well as payload functions such as winches and cranes from a distance of up to 1,000 metres. This allows marine crews to operate the vessel from the best vantage point, increasing safety and efficiency. For example, a tug operator can leave the wheelhouse to operate the vessel from a location with better visibility. 


Michael Johnson, CEO and founder of Sea Machines, said: “This continued partnership is significant because it brings together a foremost marine power and propulsion solutions provider and the leading developer of advanced and AI-based vessel control systems. Our alliance not only increases access to intelligent technologies that can positively impact operators’ bottom lines, productivity, eco-stewardship and safety, but it also provides proof of the growing market demand for these types of systems for real-world operations. We thank Rolls-Royce for their continued trust in our technology and look forward to seeing them in use aboard a variety of vessel types globally.” 


Denise Kurtulus, Vice President Global Marine at Rolls-Royce business unit Power Systems, said: “I am excited to see how quickly the teams of Rolls-Royce and Sea Machines have turned our joint vision into products available for our customers. This addition to our mtu NautIQ product portfolio is an important part of our journey towards a provider of integrated sustainable solutions. And it’s a fantastic example of how we, as a company with long history and tradition, implement cutting-edge technology – which benefits our customers and the environment alike – in a very agile way.”


Rolls-Royce business unit Power Systems, with its product and solution brand mtu, is pioneering climate-friendly propulsion and power solutions in the marine market. It is currently transforming itself from an engine manufacturer to a provider of integrated sustainable solutions. With the sustainability programme “Net Zero at Power Systems”, Rolls-Royce Power Systems is taking concrete steps towards climate-neutral solutions. For example, starting in 2023, the company will release its mtu Series 2000 and 4000 engines for sustainable fuels such as e-diesel and second-generation biofuels, thus enabling climate-neutral operation in all applications. In addition to using sustainable fuels, the company is also working on new technologies such as CO2-free fuel cell systems.

Press photos are available for download fromhttps://www.mtu-solutions.com/eu/en/news-and-media/media-center.html

About Sea Machines

Headquartered in the global tech hub of Boston and operating globally, Sea Machines Robotics, Inc. is the leader in pioneering autonomous command and control and advanced perception systems for the marine industries. Founded in 2015, the company builds autonomous vessel software and systems, which increases the safety, efficiency and performance of ships, workboats, and commercial passenger vessels. Learn more about Sea Machines at www.sea-machines.com.

About Rolls-Royce Holdings plc

  1. Rolls-Royce pioneers the power that matters to connect, power and protect society. We have pledged to achieve net zero greenhouse gas emissions in our operations by 2030 (excluding product testing) and joined the UN Race to Zero campaign in 2020, affirming our ambition to play a fundamental role in enabling the sectors in which we operate achieve net zero carbon by 2050.
  2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 9,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids and is intensively engaged in the development of climate-neutral solutions. 
  3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces and navies, and more than 5,000 power and nuclear customers.
  4. Annual underlying revenue was £10.95 billion in 2021, underlying operating profit was £414m and we invested £1.18 billion on research and development. We also support a global network of 28 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research. 
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE:RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).

Contacts

Rolf Behrens 行业媒体保护发言人
电话:
+49 7541 90 3461
电子邮件: