Rolls-Royce has delivered three mission critical mtu diesel generator sets at cost for two Indus Hospital & Health Network (IHHN) facilities in Karachi and Lahore, Pakistan to provide emergency backup power in the event of a power interruption. In the picture: Indus hospital in Lahore.Rolls-Royce hat drei mtu-Notstrom-Dieselaggregate für zwei Einrichtungen des Indus Hospital & Health Network (IHHN) in Karachi und Lahore in Pakistan zum Selbstkostenpreis geliefert, um im Falle eines Stromausfalls eine Notstromversorgung bereitzustellen. Im Bild das Indus-Krankenhaus in Lahore.
新闻稿 发电

Rolls-Royce supplies mission-critical mtu generators for non-profit hospital in Pakistan

发布于 2022年2月14日

图片 [1 文件, 2 MB]

  • Not-for-profit Indus Hospital & Health Network provides free healthcare service through its network of hospitals, care centers, and programs
  • Three mtu diesel generator sets to provide backup power at two Indus healthcare locations

Rolls-Royce has delivered three mission critical mtu diesel generator sets for two Indus Hospital & Health Network (IHHN) facilities in Karachi and Lahore, Pakistan to provide emergency backup power in the event of a power interruption. IHHN is a not-for-profit healthcare network that relies on public and corporate donations and grants to provide free and quality healthcare to millions of patients. Rolls-Royce provided the generator sets at cost to IHHN.

An mtu 18V2000 DS1400 generator set was delivered to IHHN’s Korangi Campus in Karachi and both an mtu 16V4000 DS2500 and 16V2000 DS1100 generator set to the IHHN - Qarshi Foundation, Naimat Saleem Trust & SM Pervez Campus in Lahore.

“We have done an extensive study of all reputable genset manufacturers and selected mtu gensets from Rolls-Royce due to their high fuel efficiency and excellent sales and aftersales support from R.A. Engineering & Services here in Pakistan,” said Sajid Hazrat Khan, Electrical Managers, IHHN.

“The gensets offer a high availability and reliability of power with long maintenance intervals. These technical and performance capabilities of the mtu gensets, along with low lifecycle costs made Rolls-Royce the best choice for IHHN”, said Bahir Olcay from Rolls-Royce Power Systems.

Starting with only one hospital in Karachi in 2007, IHHN has now evolved and has been working to improve healthcare in Pakistan. IHHN consists of 13 hospitals – five owned and managed by IHHN, and eight managed by the Network under the umbrella of public-private partnership – plus four regional blood centers, four physical and rehabilitation centers, Pakistan’s largest Pediatric Oncology Unit, primary care centers, and a large number of public health initiatives across the nation.

IHHN has set up container-based community health centers in Sindh and Punjab and a ‘Boat Clinic’ to serve the population of Southern Punjab. The Network is currently serving more than 450,000 patients monthly.


About Rolls-Royce Holdings plc
  1. Rolls-Royce pioneers the power that matters to connect, power and protect society. We have pledged to achieve net zero greenhouse gas emissions in our operations by 2030. We joined the UN Race to Zero campaign in 2020, and have committed to ensuring our new products will be compatible with net zero operation by 2030, and all products will be compatible with net zero by 2050.
  2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 9,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids.
  3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces and navies, and more than 5,000 power and nuclear customers.
  4. Annual underlying revenue was £11.76 billion in 2020 and we invested £1.25 billion on research and development. We also support a global network of 28 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE:RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).

Contacts

Silke Rockenstein 行业媒体发言人
电话:
+49 7541 90 7740
电子邮件: