mtu drive solution from Rolls-Royce for new modular vehicle concept ‘BOXER tracked’ from KMW
发布于 2022年6月15日
- mtu Series 880 engine powers new ‘BOXER tracked’ concept that can be equipped with Boxer mission modules
- mtu engines as a basis for mobility, reliability and simplified logistics
- Rolls-Royce presents mtu drive solutions for governmental customers at Eurosatory (hall 6, booth K568)
mtu engines from Rolls-Royce deliver the power for an innovative modular tracked vehicle concept that Krauss-Maffei Wegmann (KMW) is presenting at the Eurosatory defence technology trade fair (13 to 17 June 2022 in Paris). ‘BOXER tracked’ is the basis for a completely new family of tracked vehicles that can be equipped with the mission modules of the proven Boxer wheeled vehicles. The aim of the in-house development was to develop a highly flexible, reliable, cost-effective and rapidly available solution for the requirements of NATO and other allied armed forces. In doing so, KMW builds on proven mtu technology for the drive system: the demonstrator, which will be shown for the first time at Eurosatory, is powered by an mtu Series 880 engine, which has proven itself many times over in vehicles of the German armed forces and allies. A more powerful version of the engine will later power production vehicles. The successful Boxer vehicle family, whose mission modules are to be used in the ‘BOXER tracked’, is also powered by mtu engines.
Paul Röck, Director Sales Governmental at Rolls-Royce business unit Power Systems, said: “BOXER tracked is a very well thought-out and promising project that can only work with a drive system that is as powerful as it is reliable and easy to maintain. With our proven mtu Series 880 engines, whose power density represents the benchmark in their power range, we deliver exactly that. But this is only the beginning. We are currently developing a more powerful version of the engine for BOXER tracked, which will be suitable for all possible vehicle variants and further developments and will offer customers a high degree of future security. The performance-enhanced engine will also be excellently suited for use with a hybrid drive.”
With its mtu products, Power Systems has been a solution partner for the German and allied armed forces for drive, propulsion and energy supply for many years. The company is currently transforming into a provider of integrated sustainable solutions. In the future, climate-friendly products – such as engines for use with sustainable fuels, hybrid drive systems and emission-free fuel cells for stationary power generation – will also play an increasing role in the governmental business. Rolls-Royce will be showing its mtu solutions for governmental customers at Eurosatory (hall 6, booth K568).
About Rolls-Royce Holdings plc
- Rolls-Royce pioneers the power that matters to connect, power and protect society. We have pledged to achieve net zero greenhouse gas emissions in our operations by 2030 (excluding product testing) and joined the UN Race to Zero campaign in 2020, affirming our ambition to play a fundamental role in enabling the sectors in which we operate achieve net zero carbon by 2050.
- Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 9,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids and is intensively engaged in the development of climate-neutral solutions.
- Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces and navies, and more than 5,000 power and nuclear customers.
- Annual underlying revenue was £10.95 billion in 2021, underlying operating profit was £414m and we invested £1.18 billion on research and development. We also support a global network of 28 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.
- Rolls-Royce Holdings plc is a publicly traded company (LSE:RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).