Testing fuel performance
Rolls-Royce approves the use of synthetic paraffinic diesel fuel, also referred to as Hydrotreated Vegetable Oil (HVO), for its mtu Series 4000 and Series 1600 gensets in power generation applications. This paper provides a detailed review of the testing of an mtu Series 4000 diesel generator set operating on standard diesel fuel as well as on HVO fuel.
System tests were conducted in the field with mobile measurement technology. Engine-only tests were performed on a test bed, generating more accurate data results. The results of the testing confirm the effectiveness of HVO as a drop-in fuel for mtu diesel generator sets. In comparing the performance criteria between diesel and HVO fuel, no significant effects on general performance were observed. In fact, several positive factors were observed when using HVO.
HVO testing showed:
- A decrease in NOx, CO₂, and PM
- Improved response to load acceptance
- Full power performance
- Decreased fuel consumption
This test was conducted using both an mtu 20V 4000 G94S engine as well as a 20V 4000 DS3000 generator set.
The assessment of this test addressed the following areas:
- Load step behavior: Diesel & HVO
- Emissions testing: Diesel & HVO
- Fuel consumption comparison
- Endurance run on HVO
Fuels tested
The testing comparison of engine generator set performance was conducted using distillate diesel fuel and HVO. The diesel fuel used followed DIN 51603 (B0) and the HVO fuel followed EN15940 Class A. In the U.S., engine-only tests were performed using ULSD and HVO meeting ASTM 975. The chart below also shows ASTM D975 and EN 590 for reference.