Designing Microgrids for Efficiency and Resiliency
Posted on July 30, 2021
Tom Drake
Senior Sales Manager – Gas Power Systems
Juan Matson
Senior Sales Manager – Gas Power Systems
For decades, mission-critical facilities have depended on centralized power plants owned and operated by utilities. However, the traditional model is changing. Intelligent distributed generation systems, in the form of microgrids, are providing much-needed stability to an aging power grid.
A facility’s energy demand is key to the design of a microgrid system. To ensure efficiency and resiliency, microgrids combine different components to meet a given demand, while optimizing costs.
Key components
By combining different components, a microgrid can be tailored to every customer need, providing the ideal technical and economical solution. These systems are designed to satisfy an electrical and/or thermal energy demand that is traditionally supported by the natural gas or electric utility provider. A microgrid most commonly operates in island mode, but it also can be connected to the grid.
Distributed energy resources
These include conventional resources, like natural gas or diesel generators, that convert fuel mechanically to make electricity and thermal energy as well as renewable systems, like solar and wind, that utilize natural resources.
Energy storage
Energy is held in reserve to be dispatched as needed to supplement other distributed assets. Systems include electrochemical (BESS), mechanical (flywheels), thermal (hot water) and energy conversion. This energy can come from the overproduction of renewables, or it can be stored/charged when energy is cheaper for use at times of peak cost.
Control systems
Intelligent controls are used to optimize the available assets to provide the lowest cost of electricity by automatically dispatching supply to the most efficient resource. For example, shutting down one generator when two are running at the highest load factor to increase fuel efficiency. Control systems can operate with or without dynamic control (smart grids).
A successful microgrid solution provides modularity, scalability, energy dispatchability, power management and balancing of resources. Whether off-grid or on-grid, these powerful and reliable distributed energy generation systems can provide high performance under any site condition.
Global demand for new solutions
The energy world is undergoing a transformation. Various factors are driving growth in energy demand, and encouraging the development of flexible, sustainable, cost-effective energy solutions like microgrids. As a result, microgrid capacity and revenue continues to rise all over the world.
Benefits of microgrids and energy storage
By combining renewable power generation, power storage and conventional power generation to meet energy demands, microgrids can provide cost savings, reliability and sustainability.
Energy cost optimization
- Electricity cost reduction
- Fuel and O&M cost reductions
- Independence from electricity price development
Access to power
- Access to electricity in remote areas
- Increase of industrial load despite grid limitations
- EV charging in urban areas
Quality and security of supply
- Backup during power outages
- Voltage and frequency stabilization
- Reduction of fuel dependence
Positive environmental impact
- Increased energy use from PV & wind: reduced carbon footprint
- Incentives, tax benefits, fines avoidance
- Reputation
New revenue streams
- Revenues from grid services and energy markets
- Improved marketability of renewable energy
Implementation challenges
Every microgrid is different. To deliver the right energy mix for a facility’s needs, several key parameters must be considered in the design stage.
Reliable and economical operation
- High penetration levels of intermittent generation in stand-alone mode of operation
Schedule and dispatch of units
- Supply and demand uncertainty and determination of appropriate levels of reserves
Demand Side Management (DSM)
- Design appropriate DSM schemes to allow customers to react to the grid needs and drives supply
Distribution Level Protection
- Re-engineering of DLP schemes to account for bidirectionalpower flows
Market/business models design
- New models to allow competitive participation of intermittent energy sources driven by fuel savings
Plug and play development
- Market and control mechanisms that exhibit P&P Feature to allow for seamless integration over time
Voltage/frequency control
- Development of control techniques to account for the increase in Power-Electronics-Interfaced DG
Grid code
- Addressing grid compliance issues for the grid connectionof microgrids
Market conditions for distributed generation
Economic growth and population growth are increasing the demand for power. Increased pressure to decarbonize, and growing demand for more flexible, sustainable, cost-effective energy solutions are guiding governments and industry away from traditional energy sources like coal and gas, and toward renewable energies such as solar and wind power.
Four trends are transforming the energy world, triggering demand for new solutions:
Globalization
- Increased mobility and energy needs
- Higher level of price competition
- Urbanization
Decarbonization
- Decentralization
- Energy transition
- Increase of fluctuating renewable sources
- Environmental awareness
Electrification
- Rising electricity demand
- Increasing power need
- Environmental awareness
- Sector coupling
Digitalization
- New business models
- Increased computing performance
- High data volume and energy need for services
Costly consequences
Systems must be in place to ensure power to communities in extreme conditions. An outdated and overstressed grid has made the network more susceptible to outages. For example, in July 2019, with only 45 minutes of notice, Con Edison had to shut down power to New York City residents when a section of its system reached a maximum capacity of 12,063 MW. In Northern California, PG&E has been proactively shutting down power through rolling blackouts to avoid the risk of fire during high-risk times of the year.
In 2019, a weather/climate event caused more than $1 billion in damages 14 different times. Total costs for that year was $45 billion. In 2020, wildfires in California and the Pacific Northwest have destroyed power transmission infrastructures, disrupted public services and caused massive financial losses. Also in 2020, a storm in Iowa cut power to more than 400,000 people. Estimated damages due to lost crops are $3.7 billion, along with $82 million in home damages. For data centers, it costs nearly $9,000 every minute an outage occurs. And healthcare facilities can average nearly $700,000 per outage.
New solutions are needed
The increase in non-dispatchable renewable generation in the form of grid-scale wind and solar has added to the overall instability of the grid. Solar power, wind power and other renewable energy sources offer key benefits, but there are some drawbacks as they are dependent on weather and time-of-day, can suffer output fluctuations, and often require major capital investment. A smart microgrid uses storage and/or complementary generation technologies to optimize the use of renewables.
Upgrades to the grid are becoming more and more important due to the overall age of the transmission and distribution network. The U.S. Department of Energy (DOE) reports that 70% of power transformers are 25 years of age or older, 60% of circuit breakers are 30 years or older, and 70% of transmission lines are 25 years or older. The average age of the country’s 40,000 miles of transmission lines is 52 years. The need for reliable, independent access to power has never been greater.
Customers, key benefits and configurations
Power
Examples: grid system operators, utilities, independent power producers
Key benefits: new revenue streams, energy cost optimization
Typical configuration:
Commercial
Examples: offices, retail, warehouses, data centers, infrastructure, transport, hotels, restaurants
Key benefits: energy cost optimization, secure and reliable power supply, access to power
Typical configuration:
Industry
Examples: agriculture, manufacturing, mining, commodities
Key benefits: energy cost optimization, CO2 avoidance
Typical configuration:
Communities
Examples: remote communities, urban district/town solutions
Key benefits: energy cost optimization, access to power, CO2 avoidance
Typical configuration:
Public
Examples: military base, healthcare, institutional, education
Key benefits: energy cost optimization, quality and service of supply
Typical configuration:
Design factors for efficiency and resiliency
In a true microgrid application, the load or energy demand is key to the design of the energy system. Designing to efficiency and resiliency means balancing these assets with the cost of operation, space available, fuel resources, and government regulations.
Lifecycle costs for distributed generation system
A power generation project is a large investment. However, upfront and other fixed costs are just a small part of the total lifecycle costs. Fuel accounts for up to 70 percent of lifecycle costs. By utilizing renewable energy sources and battery storage, a microgrid can lower fuel consumption, reducing overall operating costs while ensuring the availability of reserve power.
Distributed generation systems generally lower operating costs compared to conventional power generation techniques. Properly deploying distributed generation systems requires an analysis of the existing thermal and electrical systems, ensuing the selection of building systems that are critical to continuous operation.
Secondary fuel costs
Many microgrids use a combined heat and power (CHP) module, which can produce both electric energy and heat energy from the same fuel, thereby nearly doubling overall efficiency. Higher operating efficiencies enable CHP systems to consume less fuel while generating the same amount of power and useful thermal energyas separate heat and power systems. Compared to conventional electricity and heat generation, CHP modules reduce carbon emissions by approximately 50 percent.
The challenge in maximizing the efficiency of a cogeneration application is matching the demand for the heat byproduct with the demand for electricity. If demand for electricity is greater than demand for the heat product, then excess heat must be exhausted to a radiator or water-cooling tower, thus efficiency suffers. If demand for heat exceeds generator output (light electrical demand or high heat demand), then it will need to be scaled back to match the heat output of the generator or the process, augmented with heat from a boiler.
The perfect balance
When designing a microgrid system for any application, it is important to choose the right combination of components to balance resiliency with efficiency.
Fuel availability and emissions regulations
With a widespread distribution network, natural gas is often used for North American microgrid systems. In Latin America, where pipeline natural gas might not be available, other options are often considered. Emissions rules can limit fuel types. For example, diesel may only be used in some areas for standby and with a limited run time of 100 hours or less annually.
Wind
Strength: No fuel requirement
Solar
Strength: No fuel requirement
Gas (CHP)
Strength: Opportunity to use biogas
Weaknesses: Gas pipeline or storage required, emissions controls required in certain areas
Diesel
Weaknesses: Fuel transport/storage, high CO2 emissions, high NOx emissions, limited run hours
Energy storage
Strength: Enables integration of renewables, increase flexibility of genset
Grid connection and permitting
Each individual utility creates a set of rules that govern the process and costs of operating in parallel with its transmission and distribution system. Even when electricity is kept behind the meter, the costs and time needed to properly operate in grid parallel add additional unforeseen costs to projects. Exporting excess energy is even more costly and difficult. Analysis must be performed on how any distributed energy system will affect a relationship with the utility provider.
Wind
Strengths: No carbon emissions, federal and local incentives
Weaknesses: Not dispatchable, visual and noise pollution, capital cost
Solar
Strengths: No carbon emissions, federal and local incentives
Weakness: Large space required (greenfield sites)
Gas (CHP)
Strengths: Opportunity to use biogas, dispatchable
Diesel
Strength: Dispatchable
Weaknesses: High CO2 emissions, high NOx emissions, limited run hours
Energy storage
Strength: Federal and local incentives
Ambient conditions and plant operations
Facility load or demand will drive the size and shape of the microgrid. It is important to analyze each site individually even if the loads and designs are similar, as location affects local regulations. In addition, ambient conditions, such as high altitude and high temperature, will affect how the distributed energy resources will perform. Local codes and standards are one of the main early drivers for the design of a microgrid.
Wind
Weakness: Dependent on weather conditions
Solar
Strengths: Retrofittable, e.g. on buildings
Weakness: Dependent on weather conditions and time of day
Gas (CHP)
Strengths: Power heat and cooling, efficient, economic continuous operation
Diesel
Strength: Fast start time (<20 seconds)
Weaknesses: High operating and maintenance costs
Energy storage
Strengths: Flexible use for various applications, low operation and maintenance cost
Weakness: Battery capacity degrades over time
Applications
Example #1:
Industrial Facility – Southeast USA
Site details
- Industrial demand response project
- Industrial process with high peak electrical loads
Challenges
- Control peak demand to reach goal of $100,000 monthly reduction in energy bill
- Microgrid controller to optimize all distributed generation assets
Solutions
- 3 x 16V4000 natural gas generators (6MW)
- 3 x 2MW/2MWh – 6MWh mtu Energy Pack
- 18.7 MW of PV
- Projected $1 million annual savings
Example #2:
Granjas Carroll de Mexico – Puebla, Mexico
Site details
- New pork processing facility for one of the leading producers in Mexico
- Continuous power project
Challenges
- Complete independent off-grid solution
- Customized automation system for plant control and remote operation
- Accommodate extension for heat recovery and use of biogas in future
Solutions
- 4 x 20V4000 natural gas generators
- 1 x 16V4000 diesel generator
- 9.7 MWel power output
- The first off-grid solution of its kind for Rolls-Royce Power Systems in the Americas
Microgrid Validation Center
Every microgrid is unique. Modeling real-world applications can ensure a microgrid and its control system is designed optimally. mtu Microgrid Validation Centers offer highly flexible simulation and testing capability. Equipped with diesel and co-generation standby generator sets, solar panels, mtu EnergyPack battery storage and integrated mtu automation system, the self-sustaining Validation Centers can simulate a wide range of conditions, including off-grid operation. Located in Aiken, South Carolina and Friedrichshafen, Germany, they are effective proving grounds for customers to apply a software model to just about any real-world installation.
Conclusion
Power security for mission critical facilities has traditionally been limited to a coal-fired central power plant that supplies electricity through a transmission and distribution system with on-site standby generators for selected loads, but trends are changing.
End users are paying more attention to how they design and purchase their power systems. Intelligent distributed generation systems in the forms of microgrids increase security and efficiency by offering a wide selection of power generation and storage sources, providing maximum control for facility managers, and reducing reliance on utilities.
Connect with Us
![](/etc/clientlibs/mtu/mtu-app/assets/images/_blank.gif)