Auf Europas größtem Verschiebebahnhof werden täglich Güterzuglokomotiven bis zu 4.000 Waggons sortiert und zusammengestellt.
STORY Rail

King of the hill

Posted on November 30, 2011, Images by Robert Hack

Up to 4,000 wagons are shunted around every day at Europe´s biggest marshalling yard. Without reliable freight locomotives, everything would come to a standstill.
Maschen, Germany
Goods trains arriving from different places are re-sorted at the Maschen marshaling yard.
All processes at the marshaling yard are electronically controlled. Hill supervisor, Peter Bagdahn, only has to check that the trucks roll onto the right sorting tracks.
The content of the stories reflects the status as of the respective date of publication. They are not updated. Further developments are therefore not taken into account.

Point of contact

Aaron Haussmann
Phone:
+49 7541 90 7778
+49 7541 90 77784
E-mail:

Related stories

Rail

"We could already be saving 90% of CO₂ today – but we prefer to discuss it."

A conversation with Dr. Olaf Toedter (Head of New Technologies and Ignition Systems at the Karlsruhe Institute of Technology) and Jörg Schneider (Head of Sustainability at DB Cargo) about HVO, eFuels, and the technologies that no one can see yet.

Read more

Rail

Cruise Train on rails

Superlative in every respect, the Train Suite Shiki-Shima is powered by electricity generated by two mtu Series 4000 engines on non-electrified routes.

Read more

Rail

mtu Power for Heavy-duty Steelworks Locomotives

As many as 28 locomotives are available for operation at the voestalpine Steel Division plant in Linz. Four of them are Gmeinder type D60 C marshaling locomotives each driven by an mtu Series 1600 engine. The locomotives operate on company premises hauling trains that can weigh up to 3,000 tonnes each. Two more units of the same type are on order with delivery scheduled by the end of 2015. The locomotives are operated by logistics company LogServ, a wholly-owned subsidiary of voestalpine Stahl GmbH.

Read more