Lithuanian Railways overhauls freight locomotives using MTU reman engines.
STORY Rail

Baltic revival

Posted on March 17, 2016, Images by Andzej Mickevic

Lithuanian Railways overhauls freight locomotives using mtu reman engines.
Vilnius, Lithuania

Each of the 44 mtu engines that had been powering Siemens Eurorunner locomotives in Lithuania for the last eight years had 24,000 hours of service on the clock. So it was time for a rejuvenation treatment – or, to put it another way, the mtu reman process. This involves restoring the engines to as-new condition. Remanufactured or 'reman' engines are as good as new ones but considerably less expensive and still come with the same warranty.

44 locomotives in Lithuanian Railways' locomotive fleet were remanufactured through mtu distributor Baltic Marine Group.

Economical and sustainable

In July 2013, Lithuanian Railways launched a joint project with Siemens, Baltic Marine Group and mtu to overhaul the 44 locomotives and engines. By September 2015, all of the engines, each of which had completed roughly 24,000 hours of service to date, had to be successively removed from the locomotives at the Vilnius depot and sent by truck to the mtu Reman Technology Centre in Magdeburg, mtu’s lead facility worldwide for standardized reman processes. The plant specializes in remanufacturing, i.e. standardized industrial reconditioning and complete overhaul of mtu engines. The advantage of reman engines is that they cost less than new units but have the same warranty. What is more, in the course of the complete overhaul, each engine benefits from all technical upgrades so that clients can be certain they are receiving a product with the very latest technical advances. In Magdeburg, the incoming engines are made fit and ready for a new life. The first part of the process is to completely dismantle and examine them. Wear parts and elastomer or defective components are replaced, but the majority of the engine parts such as cylinder heads, crankshafts or the crankcase are reconditioned – which is a sustainable process because no raw materials have to be used to produce new components. After successfully completing a bench test, the engines are also repainted, which means they not only meet the same specifications as an equivalent model just off the production line, they also look brand new. Just like the reman unit in locomotive number ER 20032. The Eurorunner’s 2,000 kW traction unit shines brightly in its freshly applied blue livery and is once again fully prepared for service on Lithuanian freight routes.

A 16-cylinder mtu engine has completed 24,000 hours of duty in the Lithuanian Railways freight locomotive ER 20016. Now it is being replaced by an mtu reman unit.
Giedrius Pranckunas of Baltic Marine Group lifts the old engine out of the locomotive by crane.
Andžej Mickevič (left) examines the engine together with Arunas Žėkas before the mighty unit is shipped to the mtu Reman Center in Magdeburg by road.
As good as new: the basic components such as cylinder heads, crankshafts and engine block have been reconditioned. Only wear parts and defective components have been replaced with new ones.

Out of the locomotive and onto the wooden pallet inside two minutes

In the locomotive shed in Vilnius, Arunas Žekas and Giedrius Pranckunas of the Baltic Marine Group service team are in the process of lifting the old engine out of ER 20016. Giedrius Pranckunas moves the big yellow overhead gantry crane over the locomotive by remote control. By the time it is in position, his colleague Arunas Žekas has attached heavy lifting chains to the engine block. Within a few moments, the heavyweight is hanging from the hook and being carefully lifted out of the locomotive. The fact that it seems to sway quite considerably in the process does not worry the experienced mechanics – apparently that is quite normal. Finally the engine is hovering just an arm’s width over the wooden shipping pallet. From start to finish the operation has hardly taken two minutes. Now some high-precision manoeuvring is required to position the steel colossus on the four bolts of the wooden base. "That’s no problem," smiles Arunas Žekas. "After 30 engines, it’s just a routine operation for us." The two mechanics rock the engine a little and very soon it has seated itself satisfactorily. Arunas Žekas grabs a large spanner and tightens the nuts onto the bolts.

At the mtu Reman Centre in Magdeburg, engines are remanufactured in a standardized process. First of all, they are dismantled and the components cleaned. Wear parts are replaced and all other components...
as the crankcase and conrod caps...
or the crankshaft – are reconditioned.

“The engines are in good hands"

The reman project in Lithuania took two years to complete, and Naglis Vyšniauskas is more than satisfied: "We not only have a partnership, we also have a really close collaborative relationship with mtu and Baltic Marine Group. In these two companies we have partners we can rely on." Naglis Vyšniauskas saw that trust vindicated when mtu invited its partners to the Reman Technology Centre in Magdeburg. "I was glad to see that our engines are in good hands. The plant there has high-tech equipment of the very best quality. And in our discussions I also found out how the mtu experts assess the condition of our engines after such a long period of duty. The positive feedback from mtu about the condition of our engines and, therefore, the standard of work of our maintenance staff gave me a very good feeling."

The content of the stories reflects the status as of the respective date of publication. They are not updated. Further developments are therefore not taken into account.

Point of contact

Hermann Schirmer
Phone:
+49 7541 90 4864
E-mail:

Related stories

Rail

"We could already be saving 90% of CO₂ today – but we prefer to discuss it."

A conversation with Dr. Olaf Toedter (Head of New Technologies and Ignition Systems at the Karlsruhe Institute of Technology) and Jörg Schneider (Head of Sustainability at DB Cargo) about HVO, eFuels, and the technologies that no one can see yet.

Read more

Rail

Cruise Train on rails

Superlative in every respect, the Train Suite Shiki-Shima is powered by electricity generated by two mtu Series 4000 engines on non-electrified routes.

Read more

Rail

mtu Power for Heavy-duty Steelworks Locomotives

As many as 28 locomotives are available for operation at the voestalpine Steel Division plant in Linz. Four of them are Gmeinder type D60 C marshaling locomotives each driven by an mtu Series 1600 engine. The locomotives operate on company premises hauling trains that can weigh up to 3,000 tonnes each. Two more units of the same type are on order with delivery scheduled by the end of 2015. The locomotives are operated by logistics company LogServ, a wholly-owned subsidiary of voestalpine Stahl GmbH.

Read more