Rolls-Royce is expanding its production capacity in the US with a $75 million investment in its plant in Aiken, South Carolina. The investment will primarily benefit the production of mtu Series 4000 engines, especially for the rapidly growing American data center industry. The plant will be expanded by around 37,000 square feet, creating 60 new jobs in the United States.Rolls-Royce baut seine Produktionskapazitäten in den USA mit einer Investition von 75 Millionen US-Dollar in das Werk in Aiken, South Carolina aus.  Die Investition kommt vor allem der Produktion von mtu-Motoren der Baureihe 4000 zu Gute, insbesondere für die schnell wachsende amerikanische Rechenzentrumsbranche. Die Fläche des Werks wird um rund 3.400 Quadratmeter vergrößert, wodurch 60 neue Arbeitsplätze in den Vereinigten Staaten entstehen.
PRESS RELEASE Power Generation

Rolls-Royce increases U.S. manufacturing capabilities in South Carolina

Posted on July 15, 2025

Images [3 Files, 2 MB]

  • $75M investment and creation of 60 jobs to increase production of mtu Series 4000 engines
  • New in-country machining capabilities
  • Combined $100M investment in American facilities to support data center industry growth and need for resilient, U.S.-built power

Rolls-Royce (LSE: RR., ADR: RYCEY) today announces it is expanding U.S. manufacturing capabilities with a $75M investment in its Aiken, South Carolina engine plant for mtu Series 4000 production. The investment will increase machining capabilities and grow the facility’s footprint, creating 60 new jobs in the United States with a total of 434 full-time positions at the facility. The South Carolina Coordinating Council for Economic Development approved job development credits related to the project. 

Earlier this year, Rolls-Royce announced a $24M expansion of its Mankato, Minnesota facility, adding 100 jobs to its Power Systems division in the U.S. These investments reflect the rapid growth of data centers in the U.S., increasing pressure on electric grids and the critical need for reliable power generation. 

Demand for high-power mission critical backup generators from Rolls-Royce has grown considerably over the past decade. The mtu Series 4000 engines that power these systems are built in Aiken and then assembled into complete generator sets at the Rolls-Royce facility in Mankato.

Adam Wood, Managing Director for Rolls-Royce’s Power Systems division in America said: “The increased investment strengthens our ability to serve our U.S. customers – especially in the fast-growing American data center industry. By increasing our machining capabilities in Aiken, we can supply more engines to Mankato, enabling us to deliver more gensets with shorter lead times. These investments reflect our commitment to supporting U.S. customers with reliable, locally produced solutions.” 

With this investment, Rolls-Royce will machine additional mtu Series 4000 components in the U.S. Currently, most of the components are machined in Germany and sent to the U.S. as finished goods. To meet demand, additional in-country machining is essential.

Henry McMaster, Governor of South Carolina said: “Rolls-Royce’s expansion in Aiken County further positions South Carolina as a leader in advanced manufacturing. This investment and the 60 jobs it will bring represent a big win for the community, and we are proud of the success Rolls-Royce has found in our state.”

The facility will be expanded in two phases. Phase one will grow the existing manufacturing footprint by 37,000 sq.ft. In a potential further phase, another 22,000 sq. ft. of manufacturing space could be added (60,000 sq. ft. in total). Construction for Phase 1 will begin in Q1 2026 with production set to begin in July 2027.

Adam Riddle, CEO, Rolls-Royce North America, said: “Today’s announcement underscores Rolls-Royce’s commitment to the U.S. market and demonstrates our robust manufacturing capabilities. We are proud to support America’s growing demand for reliable, domestically made energy systems that strengthen our nation’s energy independence and security. With more than half the world’s hyperscale data centers located here in the U.S., this will continue to be a key growth market for many years to come.”

Last year sales of power generation products for the data center segment grew almost 50%. As much as $1 trillion is expected to be spent globally on AI data centers, components and associated infrastructure over the next few years. In addition to data centers, Rolls-Royce provides high performance backup generators to power critical U.S. infrastructure including hospitals, municipalities and government installations.

Since the start of production in 2010, Rolls-Royce’s Aiken campus has been the site of continuous innovation and expansion. It now encompasses a 395,000 square foot campus with state-of-the-art production capabilities, an engine testing facility, office space, a research and development center, four large engine test stands and a remanufacturing and overhaul center. In 2017, the company added a 1.35 MW ground-mounted solar array on approximately 7 acres and has an additional microgrid that generates enough solar power from panels on its covered parking lot to supply its entire administration building.

The Aiken facility pioneered a nationally recognized High School Apprenticeship Program which was the first-ever vocational apprenticeship program for high school students in the state, training more than 70 students since its inception in 2012. Modelled after the German dual-education system to help cultivate the next generation of skilled manufacturing professionals, successful graduates earn certifications recognized by both the U.S. Department of Labor and Apprenticeship Carolina. 

Rolls-Royce’s transformation program is enabling it to deliver on its strategic choices. The investment in Aiken is an example of that transformation in action, as it supports the company’s strategic initiative to grow its power generation business.

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Wolfgang Boller Spokesman Regional and Business Media
Phone:
+49 7541 90 2159
E-mail: