Rolls-Royce supplies mtu large-scale battery storage to secure the Latvian national grid
Posted on February 29, 2024
- Latvia synchronizes its electricity grid with the European grid in 2025
- Large-scale battery storage system from Rolls-Royce ensures stability of the power grid in Latvia
- Transmission system operator AST orders 160MWh mtu EnergyPack
- Facility will be one of the largest battery storage systems in the EU
Rolls-Royce has received an order from the Latvian transmission system operator Augstsprieguma tikls (AST) to supply an mtu large-scale battery storage system to secure the Latvian power grid. In 2025, Latvia, together with the other Baltic states, will synchronize its energy supply system with the continental European power grid. "We are proud to be able to make a significant contribution to this important and safety-critical project in Latvia. Our battery solutions, which belong to our strategic business fields, make a sustainable and reliable contribution to energy security worldwide. The facility for Latvia will be our largest battery storage system to date," explained Dr. Jörg Stratmann, CEO of Rolls-Royce Power Systems.
Rolls-Royce will supply an mtu EnergyPack QG large-scale battery storage system with an output of 80 MW and a storage capacity of 160 MWh. This makes the system one of the largest battery storage systems in the EU. The order also includes general contractor services as well as installation and commissioning. The battery system will be used as of fall 2025 at two locations - a 20 MW/40 MWh battery storage at the AST substation in Tume and a 60 MW/120 MWh battery storage at the AST substation in Rezekne. The state-of-the-art battery system will provide the fast and automatically activated frequency regulation reserves needed for the synchronization mode, where the Baltic power transmission systems operate in sync with the continental European grids. The battery system will provide the power reserves at significantly lower costs than the existing conventional power plants. Rolls-Royce and AST have signed a 5-year Long-term Service agreement for the system.
"The battery storage systems are very important for our future energy system. I am delighted that it is being supplied by one of the world's most renowned manufacturers of energy storage systems", said Rolands Irklis, Chairman of the Management Board of AST.
"In addition to battery container solutions, Rolls-Royce supplies these mtu EnergyPack QG large-scale storage solutions, which consist of modular units for capacity and power and can be flexibly configured to any size. We look forward to working with AST and appreciate the trust that the Latvian transmission system operator has placed in us," explained Andreas Görtz, President Sustainable Power Solutions at Rolls-Royce Power Systems. The components include integrated battery cabinets and the mtu EnergetIQ intelligent control system. They are primarily used for grid services, energy trading and the integration of renewable energies. The mtu EnergetIQ control platform ensures optimum performance and flexibility.
About Rolls-Royce Holdings plc
- Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
- Rolls-Royce has a local presence in 48 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
- Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
- Annual underlying revenue was £17.8 billion in 2024, and underlying operating profit was £2.46 billion.
- Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69)5.
- Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.
Contact
Phone: |
+49 7541 90 7740
|
E-mail: |