Rolls-Royce awarded second contract to supply mtu generator sets for U.S. Navy frigate program
Posted on March 22, 2023
- mtu Series 4000 marine gensets to be manufactured inthe US; adding facility upgrades, additional jobs at two production locations
- Seamless transfer of state-of-the-art naval genset technology from Germany to US
The Power Systems division of Rolls-Royce (LSE:RR., ADR: RYCEY) has been selected to supply a further four of its mtu naval generator sets for the USS Congress (FFG-63), the second ship in the U.S. Navy’s Constellation Class Guided-Missile Frigate program, previously known as the FFG(X) program. Rolls-Royce has made significant investment at its production facilities in Aiken, S.C. and Mankato, Minn. to support the program and manufacture the gensets in the US.
Rolls-Royce is currently supplying mtu gensets for the lead ship in the Constellation Class program, the USS Constellation (FFG 62), relying on its established team in Friedrichshafen, Germany, to fulfil the project. For the second ship, the FFG-63, the company has successfully transferred advanced technology and detailed manufacturing processes to the US, investing in new facility improvements and creating new jobs to enhance its Aiken and Mankato plants. This investment will not only accommodate the specific needs of the FFG(X) program but also support future potential US naval business. Among the significant investments made at the facilities are new assembly tooling and material handling equipment, upgraded hoist systems, adapted test cells and building expansion, in addition to the creation of up to 20 new jobs.
Adam Wood, Managing Director, Rolls-Royce Solutions America, said: “We’re not only proud to continue our support of our partners in the U.S. Navy but are also thrilled to bring the manufacturing of our mtu naval gensets to the US. Working with our colleagues in Germany for a seamless technology transfer to our Aiken and Mankato facilities has strengthened our ability to meet the high expectations of this project and better position us to compete for future government programs.”
The USS Congress (FFG-63) is a multi-mission warship designed for operation in littoral and blue water environments to conduct air, anti-submarine, surface and electronic warfare, in addition to information operations. The four generator sets, each rated at 3000 kWe, are based on the proven and most power-dense mtu 20V 4000 M53B engine and will provide a total power output of 12 MW for propulsion and on-board power supply.
Fincantieri Marinette Marine (FMM) of Marinette, Wisc. was awarded the build contract for the project. The completed vessel will be powered by a combined diesel-electric and gas turbine, allowing for energy-efficient diesel power generation for propulsion at normal cruising speeds with extended range, while enhancing anti-submarine capability in its extremely quiet diesel-electric configuration. When completed, the ship will be nearly 500 feet in length, accommodate up to 200 crew and be capable of speeds in excess of 26 knots, with a range of 6,000 nautical miles at 16 knots.
About Rolls-Royce Holdings plc
- Rolls-Royce develops and delivers complex power and propulsion solutions for safety-critical applications in the air, at sea and on land. Our products and service packages enable our customers to connect people, societies, cultures and economies together; they meet the growing need for power generation across multiple industries; and enable governments to equip their armed forces with the power to protect.
- Rolls-Royce has a presence in 48 countries and customers in more than 150, comprising over 250 commercial large aero engine customers, 160 armed forces and navies and approximately 40,000 active Power Systems customers. We are committed to becoming a net zero company by 2050 and we support our customers to do the same.
- Annual underlying revenue was £15.4bn in 2023, underlying operating profit was £1.6bn and free cash flow £1.3bn.
- Rolls-Royce Holdings plc is publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
- Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,500 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.
Phone: |
+1 248 560 8488
|
E-mail: |