PRESS RELEASE Corporate

Rolls-Royce awarded Baden-Württemberg environmental technology prize for innovative sliding bearing

Posted on November 05, 2021

Images [1 Files, 1 MB]

  • Grooves in bearing surface enhance lubricative oil film
  • Enables 1% fuel saving
  • Analysis of bearing sound signature enables prediction of necessary maintenance
  • Environment Minister Thekla Walker: "Innovation with great potential"  

The Rolls-Royce business unit Power Systems has developed a sliding bearing for its mtu engines that reduces their fuel consumption by 1%. That achievement has won it the Environmental Technology Prize awarded by the Ministry for the Environment in the state of Baden-Württemberg. Minister of the Environment Thekla Walker handed the prize to Dr Otto Preiss, COO and CTO of Rolls-Royce Power Systems, on 5 November 2021. The new bearings significantly reduce the amount of friction arising between bearing and crankshaft and also enable prediction of when maintenance will next be required. “This is an innovation with huge potential, because the new bearings can simply replace the existing bearings in a whole range of applications,” said Thekla Walker, Environment Minister of Baden-Württemberg, in the awards ceremony.  

The bearing surface, instead of being entirely smooth, is furbished with fine grooves, which, together with the lubricant, produce an acquaplaning-like effect which functions as an anti-friction layer. This anti-friction layer reduces, for example, the friction-induced losses arising between crankshaft and bearing by 20-35%, depending on the operating mode. The innovative bearing is the result of a collaborative effort between a small project team in Friedrichshafen, bearing manufacturer Miba, and the MontanUniversität Leoben in Austria.  

“The technology behind sliding bearings is very mature and very well established and to genuinely improve it you need outstanding engineering expertise and innovative talent. So we're very proud that along with our partners, we've succeeded in developing an optimized metal slide bearing that can be installed in our engines without the need for further modification. With just one easy production step extra, a 1% reduction in fuel consumption can be achieved that not only lowers costs, but avoids emissions,” pointed out Dr Otto Preiss, COO and CTO at Rolls-Royce Power Systems. mtu engines produced in higher volumes by the company are to be fitted with the new sliding bearing in the near future. mtu engines already in service shall be gradually retro-fitted in the course of overhauls. The future plan is for the new bearing to be marketed as an individual component by Miba AG.  

Use of the bearing in the engine reduces friction-induced losses, and while power output is maintained, fuel consumption drops by around 1%. That does not sound like very much, but a little goes a long way, as the following simplified example shows: A mining truck powered by a large engine whose power output is roughly equivalent to that of twenty medium-sized passenger cars runs for around 20 hours a day, consuming some 400L of fuel per hour under full load. Installed in the engine, the new bearing alone therefore enables a fuel saving of around 80L per day.  

Furthermore, the innovative bearing technology indicates when the next major maintenance work will be due by producing a change in the sound signature of the bearing which can be interpreted accordingly. That enables the service life of the bearing to be fully exploited. Premature maintenance is avoided and excessive wear identified in good time, saving both material and operating costs.  

The bearing, for which a patent is pending, is not only suitable for use in mtu engines from Rolls-Royce: “It is suitable for all equipment in which sliding bearings must withstand high loads – for example utility vehicle engines, turbines and wind power plants, which, thanks to the new bearing, go into operation a little more quickly than before and are therefore productive for longer,” explained Dr Thomas Kottke, who is heading up the project.

About Rolls-Royce Holdings plc

  1. Rolls-Royce pioneers the power that matters to connect, power and protect society. We have pledged to achieve net zero greenhouse gas emissions in our operations by 2030. We joined the UN Race to Zero campaign in 2020, and have committed to ensuring our new products will be compatible with net zero operation by 2030, and all products will be compatible with net zero by 2050.
  2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 9,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids.
  3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces and navies, and more than 5,000 power and nuclear customers.
  4. Annual underlying revenue was £11.76 billion in 2020 and we invested £1.25 billion on research and development. We also support a global network of 28 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE:RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).

Contacts

Wolfgang Boller Spokesman Regional and Business Media
Phone:
+49 7541 90 2159
E-mail: