There is no question that energy is needed. The demand will increase massively in the coming years – especially for things like data centers that power our connected world. At the same time, security of supply is declining. The Ukraine war and the resulting gas crisis clearly show that both the availability and the quality of energy can no longer be taken for granted – and not just in Europe. The word needs power that can be produced reliably and climate-neutrally.
Energy storage is the big challenge
One trend is already evident and will become even more pronounced in the future: The era of large power plants is ending; energy is increasingly being generated decentrally – and more sustainably, from renewable sources such as wind and sun. The challenge is that ideal conditions do not always exist for generating power through sustainable sources precisely when it is needed. Often the sun is not shining or the wind is not blowing.. Even then, energy must be made available. "The big challenge is to store the energy from renewable sources," said Tobias Ostermaier, President of Rolls-Royce's Stationary Power Solutions division. He presented the mtu EnergyPack for this purpose: Battery containers in the 550 to 2,200 kilowatt-hour capacity range. These store energy from renewable sources and make it available when it is needed.